The page you're viewing is for Korean (Korea) region.

Vertiv 영업담당자에게 문의하시면 고객의 고유한 요구에 맞게 복잡한 설계를 구성할 수 있습니다. Vertiv는 대규모 프로젝트에 대한 기술 지침이 필요한 조직에 필요한 지원을 제공할 수 있습니다.

자세히 보기

많은 고객이 Vertiv 리셀러 파트너와 협력하여 IT 애플리케이션을 위한 Vertiv 제품을 구매합니다. 파트너는 다양한 교육을 받고 전문 경험을 보유하고 있으며 Vertiv 제품을 통해 전체 IT 및 인프라 솔루션을 지정, 판매, 지원할 수 있는 독보적인 위치에 있습니다.
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
Beyond the compressor-less hype: Matching data center cooling technology to climate reality

7 분 읽기

Despite elevated cooling temperatures, learn which cooling technologies and innovations work best based on geography, climate, external ambient conditions, water availability, and thermal differentials before making million-dollar infrastructure decisions.

As chip temperatures at the technology coolant supply (TCS) potentially reach 40-45°C/104°-113°F, many assume the industry is entering an era of universal "compressor-less" cooling—eliminating mechanical refrigeration compressors in favor of passive heat rejection, which can help reduce facility energy consumption. But the latest white paper, “Rising Chip Temperatures and the Transformation of Data Center Cooling: A Scenario-Driven Assessment of Heat Rejection Technologies”, reveals a more nuanced reality: location determines cooling technology as much as chip specifications do.

The five-zone framework

Vertiv researchers created the chilled water heat rejection map for liquid cooling, dividing the operational landscape into five distinct zones, defined by the intersection of server temperature and external ambient conditions:

  • Zone 1 (Compressor-less ideal): High server temperatures (≥30°C/86°F) combined with medium-low ambient temperatures create the sweet spot for dry coolers and adiabatic dry coolers. These systems can help reduce power consumption by eliminating compressor loads entirely. However, this zone represents a narrow slice of real-world deployments—typically limited to cold climates or facilities with elevated return water temperatures.
  • Zone 2 (Water-enabled compressor-less): Cooling towers extend the compressor-less operational field for medium-high server temperatures (≥25°C/77°F) in medium-low ambient conditions. However, this can increase water consumption and dependency on local water availability—factors increasingly constrained by environmental regulations and resource scarcity.
  • Zone 3 (Hybrid solutions): When both server temperatures and ambient temperatures run high, trim cooler technology bridges the gap. This innovative hybrid operates as a dry cooler during favorable conditions and seamlessly engages compressors as ambient temperatures climb, potentially reaching 55°C/131°F and higher. It represents operational flexibility for facilities operating in variable climate conditions.
  • Zone 4 (Mixed mechanical + free cooling): For medium-low server temperatures (≤35°C/95°F) paired with moderate ambient conditions, free-cooling chillers and water-cooled chiller + dry cooler combinations optimize efficiency by leveraging free cooling when available while maintaining mechanical backup capability.
  • Zone 5 (Full mechanical): Extreme climates with sustained temperatures above 50°C/122°F combined with medium-low server temperature requirements necessitate traditional chillers or adiabatic chillers. No amount of chip temperature elevation eliminates this need when ambient conditions exceed thermal differentials required for passive heat transfer.

Figure 1. The Chilled Water Heat Rejection Map identifies the possible technologies data center operators can use to manage their cooling needs in the facility based on crucial factors for optimized resource use and availability. Source: Vertiv.

In parallel, this research provides an overview of air-based cooling architectures and defines the operational conditions that necessitate compressor-driven mechanical cooling for room-level thermal management. This provides additional, broader context to position these requirements and to complement the liquid-cooling analysis and considerations discussed.

Figure 2. The Air Cooling Heat Rejection Map identifies three distinct operating zones for indoor chilled water units, depending on the facility water temperature and the target return air temperature, among other considerations. Source: Vertiv.

To find the complete list of factors included for consideration of thermal technologies, the definitions, and breakdown and basis of the zones, download the paper here.

Higher temperatures = Compressor-less cooling?

Given the analysis, the assumption that higher chip temperatures automatically warrant the use of compressor-less cooling solutions for efficient thermal management is a misconception that overlooks critical environmental and operational variables.

While elevated chip inlet temperatures, potentially reaching 40°C to 45°C (104 to 113°F), create greater thermal headroom for passive heat rejection, the feasibility of compressor-less technologies depends on three converging factors:

  • The working temperature on the chip or server side
  • The external ambient conditions (temperature and humidity) of the data center location, and
  • The availability of water for evaporative or adiabatic processes.

The relationship is governed by a fundamental thermal differential (Δ in/out), representing the temperature difference between server-side conditions and outdoor air. For example, if a data center operates with server temperatures at 20°C/68°F while outdoor temperatures reach 35°C/95°F, compressor-based systems remain necessary because the external air is too warm for passive cooling. Conversely, a facility operating at 40°C/104°F chip temperature in the same climate could theoretically use compressor-less dry coolers. However, in extreme climates where outdoor design temperatures consistently reach 50°C/122°F to 55°C/131°F, even 40°C/104°F chip temperatures would be insufficient to eliminate compressors as outdoor air remains hotter than the system's return temperature.

Therefore, compressor-less viability is not universally enabled by high chip temperatures alone but is fundamentally constrained by local climate and water resource availability.

The 90% reality check

Perhaps the most striking finding in our research: over 90 percent of North America's top data center markets experience design temperatures ≥40°C/104°F. While there are differences in numbers, similar patterns emerged across Europe and the Asia Pacific.

This means the vast majority of existing and planned facilities operate in climate zones (i.e., IECC Hot through Mixed classifications) where compressor-less technology faces significant limitations, even with elevated chip temperatures. A data center in Phoenix, Dubai, or Perth with 40°C/104°F chip temperatures still requires mechanical cooling, because ambient temperatures of 50°-55°C/122-131°F exceed the viable thermal differential. Conversely, facilities in Anchorage, Scandinavia, or northern regions of Japan can leverage compressor-less designs effectively.

Design for reality, not theory

The transformation of data center cooling isn't a simple equation of rising chip temperatures enabling universal compressor-less operation. It's a complex interplay of business growth objectives, thermal requirements, geographic constraints, water availability, and long-term operational resilience. The white paper provides the framework, technical specifications, and climate mapping essential for making informed infrastructure decisions worth millions in capital and operational expenditures.

Download the full research to access detailed zone analysis, regional climate maps, and technology selection matrices to find the specific deployment scenarios.


AI 인공 지능 Colocation Consultants 데이터 센터 혁신 효율성 ESG/sustainability 초고밀도화 시설 최적화 Liquid Cooling 열 체인 진화 열 관리 총 소유비용 Trends

VertivTM AI Hub

Infrastructure designed to stay multiple compute generations ahead, starting now.

Learn more
PORTALS
개요

언어 & 지역