The page you're viewing is for Korean (Korea) region.

Vertiv 영업담당자에게 문의하시면 고객의 고유한 요구에 맞게 복잡한 설계를 구성할 수 있습니다. Vertiv는 대규모 프로젝트에 대한 기술 지침이 필요한 조직에 필요한 지원을 제공할 수 있습니다.

자세히 보기

많은 고객이 Vertiv 리셀러 파트너와 협력하여 IT 애플리케이션을 위한 Vertiv 제품을 구매합니다. 파트너는 다양한 교육을 받고 전문 경험을 보유하고 있으며 Vertiv 제품을 통해 전체 IT 및 인프라 솔루션을 지정, 판매, 지원할 수 있는 독보적인 위치에 있습니다.

리셀러 찾기

필요한 것이 무엇인지 이미 알고 계십니까? 온라인 구매 및 배송의 편리함을 원하십니까? 특정 범주의 Vertiv 제품은 온라인 리셀러를 통해 구매할 수 있습니다.


온라인 리셀러 찾기

제품 선택에 도움이 필요하십니까? 여러분에게 적합한 솔루션을 안내할 수 있는 우수한 Vertiv 전문가와 상담하십시오.



Vertiv 전문가에게 문의하기

The page you're viewing is for Korean (Korea) region.

Heat rejection cooling efficiency: Location, climate-based thermal management strategy

11 분 읽기

As artificial intelligence (AI) and high-performance computing (HPC) push chip temperatures toward 40-45°C/104-113°F, a recurring theme has emerged: higher chip temperatures automatically enable compressor-less cooling. The reality is far more complex.

Download the white paper

This white paper reexamines conventional thinking by demonstrating that effective thermal management depends on three critical factors working together:

  • Chip operating temperature 
  • Local climate conditions, and 
  • Water availability. 

Through our comprehensive Air Cooling and Chilled Water Heat Rejection Maps, we reveal why a data center in Phoenix, in Dubai or Perth operating at 40°C/104°F still requires compressors as external ambient temperatures exceed the thermal differential needed for passive cooling, while a facility in Scandinavia or in Canada at the same working temperature can leverage compressor-less technology.

Key insights covered in this white paper include:

  • The climate reality: Over 90% of North American data centers are built in regions with design temperatures ≥40°C/104°F, severely limiting compressor-less adoption regardless of chip temperature increases.
  • Operational zones: A framework identifying which cooling technologies work best based on server temperature, ambient conditions, and water use. 
  • The water trade-off: How adiabatic systems and other solutions that rely on evaporative processes, such as cooling towers and hybrid coolers, can extend compressor-less viability, but introducing water consumption, cost, and regulatory challenges. 
  • Air cooling considerations: How optimal temperature differential (ΔT) of 10-12°C/50-54°F between return and supply air make a difference, the three operational zones for indoor water units when air cooling alone becomes less efficient, and how dedicated secondary water loops may be required in the long run. 
  • Location-specific strategies: Detailed climate zone mapping across North America, Europe, and Asia-Pacific showing where different cooling approaches make practical and economic sense. 

The strategic implications are clear: Operators need to re-evaluate their infrastructure and the geographic applicability of compressor-less technologies. Whether designing new facilities or retrofitting existing infrastructure, this paper provides the strategic rationale to match the right cooling technology to the data center’s operational environment.

Learn why the path to efficiency is not one-size-fits-all and discover which solutions align with your specific temperature, climate, and water constraints.

+

AI 인공 지능 Colocation Consultants 데이터 센터 혁신 효율성 ESG/sustainability ESG/Sustainability 초고밀도화 시설 최적화 Liquid Cooling 열 체인 진화 열 관리 열 관리 총 소유비용 Trends

VertivTM AI Hub

Infrastructure designed to stay multiple compute generations ahead, starting now.

Learn more
PORTALS
개요
파트너 로그인

언어 & 지역