The page you're viewing is for Japanese (Japan) region.

Vertivの製造担当者と連携すると、複雑な設計をお客様独自のニーズに合わせて構成することが可能になります。大規模なプロジェクトに関する技術的ガイドが必要な組織に対して、Vertivは十分なサポートを提供いたします。

詳細を見る

Vertiv再販業者パートナーと連携して、多くのお客様がITアプリケーション用のVertiv製品を購入しています。パートナーは、広範なトレーニングと経験を積み、ITおよびインフラに関するソリューション全体をVertiv製品で明確にし、販売、サポートを行うという独自の立場を構築しています。

再販業者を見つける

ご自身に必要なものについて特定済みですか? 便利なオンラインショッピングおよび配送をご希望ですか? 特定のカテゴリーのVertiv製品は、オンライン再販業者を通じて購入可能です。


販売代理店のECサイトを検索

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

The page you're viewing is for Japanese (Japan) region.

Validating AI Factory design challenges with physical system-level testing

2 分 読む

AI factory economics at scale depend on validated systems instead of individual components. Learn why infrastructure must be simulated and tested as an interdependent whole before deployment.

Download the app brief

AI factories are rewriting the economics of compute infrastructure at scale. Billions in capital committed against a single operational question: can electrical capacity be converted into productive compute quickly, reliably, and at a cost structure that justifies the investment?

The answer depends on how the complete physical system behaves as a convergent whole under real-world AI workload conditions. Namely, the power trains, thermal chains, controls, software, and the interfaces between them, working in sync.

Five intensifying forces are driving this shift:

  • Density is compressing the margin for error at the rack level.
  • Speed is making time to productive capacity the defining competitive metric.
  • Scale is turning manageable interactions into dominant engineering challenges.
  • Complexity is multiplying the interfaces where design intent diverges from physical reality.
  • Dynamic workload profiles are rendering steady-state assumptions obsolete.

The traditional validation approaches of testing individual components against isolated specifications remain necessary. However, they no longer address the question operators are asking on the ground: does the system work when everything runs simultaneously?

The gaps that matter most exist at the interfaces and seams between systems.

This application brief introduces a closed-loop validation methodology that connects virtual simulation, physical systems-level testing, field deployment, and operational learning into a continuous cycle. Each iteration reduces the variance between what was designed and what is delivered.

Figure 1. The closed loop enables the continuous reduction of variance between design intent and physical and operational reality. Source: Vertiv.

It examines how decades of distributed critical infrastructure validation capability can be consolidated and focused specifically for AI factory systems: validating combined power, thermal, and control behavior at greater scale, speed, and fidelity. And it frames the economic argument around four metrics that connect infrastructure performance to AI factory outcomes.

The brief provides a capacity validation framework; the questions to ask at each phase of the lifecycle, the indicators that distinguish validated confidence from inherited assumption, and the engineering logic behind treating infrastructure as a system rather than a collection of parts.

The infrastructure either performs as a validated system or performs as an assumption. AI factory economics leave increasingly little room for the latter.


AI All Services 人工知能 Availability & Uptime Cloud Computing Colocation Critical power データセンターのイノベーション デジタルファースト設計 Edge Efficiency 超高密度化 Facility Optimization ギガワット規模のキャンパス Liquid Cooling Maintenance Testing Monitoring 電源アーキテクチャの変革 Services Unified Infrastructure
Partner Login

言語と地域