The page you're viewing is for Spanish (LATAM) region.

Al trabajar con el soporte de ventas de Vertiv, puede configurar los complejos diseños de acuerdo con sus necesidades específicas. Si forma parte de una organización que busca orientación técnica para un proyecto grande, Vertiv puede ofrecerle el soporte que necesita.

Más información

Muchos clientes trabajan con un socio revendedor de Vertiv para comprar productos de Vertiv para sus aplicaciones de TI. Los socios cuentan con amplia capacitación y experiencia, y están en una posición única para especificar, vender y brindar soporte a soluciones completas de TI e infraestructura con los productos de Vertiv.

Buscar un revendedor

¿Ya sabe lo que necesita? ¿Desea la comodidad de comprar y enviar en línea? Ciertas categorías de productos de Vertiv se pueden comprar a través de un revendedor en línea.


Encontrar un vendedor en línea

¿Necesita ayuda para elegir un producto? Hable con un especialista de Vertiv altamente calificado, quien le guiará hacia la solución adecuada para usted.



Contactar a un especialista de Vertiv

The page you're viewing is for Spanish (LATAM) region.

The German Climate Computing Centre (DKRZ), located in the centre of Hamburg, is renowned by climatologists from around the world.

Here, a team of nearly 80 employees combines technical expertise and special high performance computers to perform complex climate simulations for research purposes. As these simulations require significant computing and data storage capacities, DKRZ has been continuously improving its computing power in order to stay abreast in an evolving and competitive industry. With the installation of a new high performance computing system, Mistral, in summer 2015, DKRZ has seen performance increase twentyfold, at a lower power consumption. The investment into increased computing power and storage capacity has helped to make DKRZ one of the world’s elite computing centres for climate research.

Case Summary
Location:

Hamburg, Germany

Critical Need:

DKRZ was faced with the challenge of upgrading its computing power in an efficient way to ensure reliable and failure-free operations for its new mainframe computer, Mistral. The computer’s energy consumption constantly changes, and can deviate up to 50 percent within fractions of a second. As a result, it was necessary to equip the existing computing centre with a completely new infrastructure, including an uninterruptible power supply (UPS) capable of bridging temporary current fluctuations with ease.

Vertiv Solution:

The Liebert Trinergy Cube configuration at DKRZ is particularly unique. By interconnecting a total of six 400 kVA modules, a single UPS system provides 2400 kVA of power. However, this is only one example of numerous technical advantages which the Liebert Trinergy Cube provides

Download the Case Study

Artículos relacionados

University of Southampton Image

Casos de éxito

University of Southampton
T-Systems Image

Casos de éxito

T-Systems
Iniciar Sesion Como Socio

Idioma y ubicación