Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Federal Government Solutions

With years of successfully partnering with federal customers, Vertiv's dedicated federal team is there to guide you. At every turn, we will guide you through finding the best solutions for your needs. Our wide portfolio of power, thermal, management, services and monitoring solutions come with continued support to help you from implementation all the way through troubleshooting. We'll work with you to make managing and maintaining your critical technology a breeze.

Is your government AI-ready? 

Government AI applications demand new data center capacity for secure, efficient data processing and AI data center cooling.

Learn more

Infrastructure challenges

Reliable remote access and control

  • With a new breakdown of workers still in the office and at home, IT managers now require remote access and control to view conditions and troubleshoot where needed.
  • Downtime isn’t an option for the federal government as that would expose them to external threats. Maximizing IT security that can managed whether in or out of band is crucial.
  • The “Power of Being There” no matter your location has never been more relevant than it is today. Helping customers access their data centers remotely is in our DNA.

Easily integrated and scalable infrastructure

  • With changing budgets every year, federal agencies need to scale up quickly to meet their new demand.
  • An agency may not have the budget one year but need to scale up quickly the next. Investing in flexible rack and containment solutions early makes it easy for customers to scale when needed.
  • Mainly purchasing IT assets during a short buying season means ease of purchase is top of mind for agency personnel. Integrated solutions are a great way to simplify the purchasing process.

Remote and on-premise security

  • IT managers must ensure that sensitive data and information are protected against cyber-attacks and other threats.
  • A federal agency’s IT assets must be protected in its entirety, from hardware to software.
  • At every level, data and assets must be protected through centralized monitoring for maximum security and ease of management.

TAA/BAA compliant solutions

View products

The Vertiv™ Cybex™ Secure MultiViewer

The Vertiv™ Cybex™ Secure MultiViewer KVM is ideal for environments where monitoring and managing of multiple active computers, covering various degrees of secure data is required. Through Cursor Navigation Switching (CNS), users have the flexibility to manage and monitor their data by simply holding down the left CTRL key and moving their mouse across window borders. Offering a dual head option, the MultiViewer enables the user to monitor up to 4, 8 or 16 computers on dual displays.

Learn more

Vertiv™ Liebert® GXT5 UPS

1000-3000VA / Online Double Conversion UPS / Single-Phase

The Vertiv™ Liebert® GXT5 TAA UPS is an online double conversion UPS solution which offers premium power outage protection and continuous power conditioning in a compact and flexible rack/tower form factor.

Get brochure

Vertiv™ SmartMod™

Vertiv™ SmartMod™ is a flexible platform, optimized for simplified deployment of critical IT assets. For small room IT deployments up to 10 racks and 100kW or less, SmartMod offers a simple way to install capacity in a fraction of the time a typical IT build might take.

Product Highlights:

Get brochure

Liquid cooling solutions

Data center operators are pursuing one of three paths with liquid cooling. They’re developing liquid-only data centers, future-proofing air-cooled facilities with new infrastructure to support liquid-cooled racks in the future and integrating liquid cooling in current air-cooled facilities that lack the infrastructure to support it. Most will likely choose the latter path, to gain capacity that meets near-term business needs and provides rapid return on investment.

Learn more

Vertiv™ Liebert® APM2

Introducing a next-generation modular and transformerless UPS design, Vertiv™ Liebert® APM2 , a feature-rich high-density UPS that brings exceptional and innovative features for mission-critical applications. Powered by latest generation three-level IGBT topology in conjunction with Silicon Carbide converter, it delivers an extraordinary double conversion efficiency of up to 97.5% that ensures remarkable operational cost savings, reducing both the Total Cost of Ownership (TCO) and the environmental impact.

Get brochure

Vertiv™ Powerbar iMPB

Ideal for dynamic data center environments, the modular Vertiv™ Powerbar iMPB allows businesses to cost-effectively optimize and adapt power distribution infrastructure over time. User friendly tap-off boxes can be placed anywhere along the busway for easy integration into any data center layout and speedy scalability. The adaptive busway design also maximizes availability with continuous power delivery to critical loads even during upgrades and changes.

Get brochure
 

Federal contracts
and capabilities

Download contracts

See us at
events

View events

 

Case study

Vertiv™ SmartMod™ Solution Enables Government Department to Scale Up New Edge Site Within Two Months

One of the UK’s largest public sector organisations came to Vertiv with a requirement to rapidly scale up data processing capacity at its Kent border site, which called for a new edge facility.

Read more

Need help selecting a solution?

Please fill out the form and we will get back to you as soon as possible.
PORTALS

Language & Location