The page you're viewing is for English (ANZ) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (ANZ) region.

Vertiv’s new pre-integrated IT rack is designed for demanding edge applications in North America and EMEA

8/5/24

Vertiv™ SmartCabinet™ ID provides power, cooling, environmental protection, and physical security in a small footprint

Westerville, Ohio [May 8, 2024] – The proliferation of edge computing use cases has shifted critical equipment and data from the protected confines of the data center to more demanding environments where heat, humidity, air quality, and physical security are significant challenges. Recognizing this new reality, Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the Vertiv™ SmartCabinet™ ID, an all-in-one, fully sealed single-rack enclosure that delivers cooling, power, and environmental protection for applications at the network edge. The SmartCabinet™ ID is available today in North America and EMEA with multiple rack sizes and cooling capacity options, including 24U and 42U racks, and 3.5 kW and 7.0 kW of cooling capacity.

The sealed SmartCabinet ID solution protects the enclosed IT equipment against dirt, dust, and fluctuating temperatures typical of warehouses, factory floors, and other common edge locations, and is IP54-rated for water-resistance, providing protection in case of indoor sprinkler system activation. Integrated emergency fans also provide backup cooling in the event of a power outage or a primary cooling module failure. A built-in touchscreen display with communication capabilities enables local or remote monitoring and control of key components, while alarms and notifications for local and remote users can be customized to alert to out-of-spec ambient conditions. Optional electronic locks can be provided on the front and rear doors, with the ability to track access and customize for authorized users.

The SmartCabinet ID addresses another challenge common to sites at the edge of the network by maximizing space utilization, a core principle of its design. Both its integrated cooling solution and the power management block, which provides power to the cooling, display, emergency fans and sensors, use zero U-space in the rack, preserving valuable space for servers and other IT equipment.

Vertiv also offers a full suite of services for the Vertiv™ SmartCabinet™ ID, including installation and startup, preventative maintenance contracts and extended warranties, providing seamless deployments and peace-of-mind for IT deployed in harsh conditions. It is also compatible with Vertiv's compact rack-mount uninterruptible power supply (UPS) systems, such as the Vertiv™ Liebert® GXT5 and Vertiv™ Liebert® GXT5 Lithium Ion, which provide power outage protection and continuous power conditioning.

“Edge compute sites such as those found in industrial, logistic and commercial environments directly enable business-critical applications, but the IT organizations responsible for their performance can be challenged to maintain the service levels commonly delivered within traditional data center facilities,” said Alex Pope, vice president of global edge systems at Vertiv. “The SmartCabinet™ ID was designed specifically to address the physical security risks and demanding environments of many edge sites, in addition to power and cooling at the capacities needed in these spaces.”

The SmartCabinet ID can be viewed virtually via the Vertiv™ XR app, an augmented reality experience that is downloaded to a mobile or tablet device. Vertiv XR app allows the user to visualize the solution in their own space and explore features and details from every angle.

Vertiv also recently announced its end-to-end portfolio for High Performance Compute (HPC) and AI deployments, Vertiv™ 360AI. The solutions include power, cooling, enclosures, end-to-end lifecycle services, and digitized management.

For more information on the SmartCabinet ID and other pre-engineered solutions from Vertiv, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

Brianna Rabe - Ruder Finn
E 
brianna.rabe@ruderfinn.com

Related Articles

PARTNERS
Overview

Language & Location