The page you're viewing is for Japanese (Japan) region.

Vertivの製造担当者と連携すると、複雑な設計をお客様独自のニーズに合わせて構成することが可能になります。大規模なプロジェクトに関する技術的ガイドが必要な組織に対して、Vertivは十分なサポートを提供いたします。

詳細を見る

Vertiv再販業者パートナーと連携して、多くのお客様がITアプリケーション用のVertiv製品を購入しています。パートナーは、広範なトレーニングと経験を積み、ITおよびインフラに関するソリューション全体をVertiv製品で明確にし、販売、サポートを行うという独自の立場を構築しています。

再販業者を見つける

ご自身に必要なものについて特定済みですか? 便利なオンラインショッピングおよび配送をご希望ですか? 特定のカテゴリーのVertiv製品は、オンライン再販業者を通じて購入可能です。


販売代理店のECサイトを検索

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

The page you're viewing is for Japanese (Japan) region.

How steel-frame modular construction cuts data center embodied carbon by more than half

14 分 読む

New Life Cycle Assessment (LCA) report quantifies the carbon advantage of prefabricated systems over traditional concrete builds and reveals where the savings actually come from.

Download white paper

How you build sets carbon locked in from day one.

While the industry focuses on power usage effectiveness (PUE) and operational efficiency, embodied carbon gets locked in before a single server powers on. And unlike energy consumption, you can't optimize it later.

Data center operators now face converging pressures: accelerating capacity demand, tightening emissions reporting requirements, customer expectations for low-carbon infrastructure, and investor scrutiny of Scope 3 emissions. The task is now to deliver capacity at speed and scale while keeping carbon impact in check.

Prefabricated modular data centers (PMDCs) have gained traction for deployment speed, but their carbon advantage has been more assumed than quantified. Until now.

What the assessment measures

A comprehensive Life Cycle Assessment (LCA) conducted according to European Standard EN 15978 compares "a 1.5-megawatt (MW) PMDC with steel-frame construction" against "a conventional concrete-shell facility with matching IT capacity." The LCA report tracks embodied carbon across material production, transport, construction, refurbishment potential, and end-of-life scenarios.

The scope deliberately excludes operational energy to isolate the carbon impact of construction decisions alone. What remains is a comparison of how building methodology drives the portion of a data center’s carbon footprint that's irreversible once construction begins.

Where prefabricated modular data center wins

The carbon advantage stems from five interconnected factors:

Material efficiency.

Steel-framed modules achieve equivalent structural performance with significantly less material mass than concrete, resulting in lower aggregate emissions.

Factory precision.

Research shows that off-site construction can lower waste to 1.8%, compared to the 30% waste generated by conventional methods.

Efficient, low-impact assembly.

Controlled factory conditions can replace energy-intensive onsite work, cut rework, and streamline logistics. Parallel workstreams can shorten deployment time by up to 50%.

Standardization at scale.

Factory-controlled production environments offer greater measurement precision and consistency.

Steel's circular lifecycle.

Steel maintains its structural integrity through repeated recycling cycles, with "over 90% recovery rates.

Why this study matters

Construction decisions made today will define the industry's carbon trajectory for decades. Understanding how building methodology shapes embodied carbon isn't just about compliance. It's about building infrastructure that scales responsibly.

The full whitepaper includes detailed methodology, life cycle stage analysis, and recommendations for emerging approaches including cross-laminated timber and green steel sourcing.

Get the full analysis, technical specifications, and carbon accounting framework.

Book a meeting modal

<

+

データセンターのイノベーション ギガワット規模のキャンパス

VertivTM AI Hub

Infrastructure designed to stay multiple compute generations ahead, starting now.

Learn more
Partner Login

言語と地域