The page you're viewing is for Italian (EMEA) region.

Rivolgiti a un rappresentante di Vertiv che lavorerà al tuo fianco e ti aiuterà a realizzare progetti complessi in base alle tue esigenze. Se la tua organizzazione ha bisogno di assistenza tecnica per un grande progetto, Vertiv può fornirti tutto il supporto necessario.

Ulteriori informazioni

Molti clienti si affidano ai reseller che sono partner di Vertiv per l’acquisto di prodotti ideali per le loro applicazioni IT. Affidati alle elevate competenze dei nostri partner che, grazie ai prodotti Vertiv, sono in grado di offrire soluzioni complete per infrastrutture e applicazioni IT: dalle specifiche alla vendita all’assistenza.

Trova un reseller

Sai già di cosa hai bisogno? Vorresti la comodità dell’acquisto e della spedizione online? Alcune categorie di prodotti Vertiv si possono acquistare tramite un reseller online.


Trova un reseller online

Hai bisogno di aiuto per scegliere un prodotto? Parla con un esperto di Vertiv altamente qualificato che ti orienterà verso la soluzione più adatta.



Contatta un esperto di Vertiv

The page you're viewing is for Italian (EMEA) region.

Spotlight: Bringing NVIDIA AI Computing Capability to the Naval Postgraduate School 

1 min. Lettura

Existing IT room conversion for high-density, liquid-cooled AI environment to support NVIDIA DGX™ GB300

The Naval Postgraduate School, the United States Navy’s graduate university and research institution, is accelerating artificial intelligence education, research, and capability delivery, and expanding the Department of the Navy’s and Joint Force’s ability to apply AI to real operational challenges. The expansion enables NPS to serve faculty, students, researchers, and mission partners addressing complex challenges through advanced computing and artificial intelligence.

Working closely with NVIDIA and a broad ecosystem of partners, Vertiv provided system-integrated power and cooling infrastructure, engineering expertise, and the deployment support required to enable the high-density liquid-cooled installation.

The project:

  • Establishes an advanced, locally operated AI environment for education, research, digital engineering, modeling and simulation
  • Demonstrates how an existing facility can be transformed to support the electrical, thermal, and operational requirements of next-generation accelerated computing
  • Supports AI-enabled education, research, digital engineering, modeling, and simulation

Read the announcement

Vertiv™ SmartIT for Enterprise 

Accelerate enterprise AI with scalable, pre-integrated rack-level infrastructure

Vertiv™ SmartIT is a pre-integrated, rack-level AI infrastructure solution for NVIDIA DGX GB300, combining Vertiv power, cooling, rack infrastructure, and commissioning into one pre-validated package ordered as one solution and delivered as one unit.

Deploy AI faster with pre-integrated solutions

Reduce integration risk with pre-engineered reference designs

Support increased rack densities of up to 142kW within existing footprints

Explore the solution


AI Intelligenza artificiale Disponibilità e operatività Critical power Innovazione nei data center DCIM e gestione IT Design incentrato sul digitale

VertivTM AI Hub

Un'infrastruttura progettata per supportare con anticipo più generazioni di piattaforme di calcolo, a partire da ORA.

Ulteriori informazioni
Login dei partner

Lingua & Ubicazione