The page you're viewing is for Italian (EMEA) region.

Rivolgiti a un rappresentante di Vertiv che lavorerà al tuo fianco e ti aiuterà a realizzare progetti complessi in base alle tue esigenze. Se la tua organizzazione ha bisogno di assistenza tecnica per un grande progetto, Vertiv può fornirti tutto il supporto necessario.

Ulteriori informazioni

Molti clienti si affidano ai reseller che sono partner di Vertiv per l’acquisto di prodotti ideali per le loro applicazioni IT. Affidati alle elevate competenze dei nostri partner che, grazie ai prodotti Vertiv, sono in grado di offrire soluzioni complete per infrastrutture e applicazioni IT: dalle specifiche alla vendita all’assistenza.

Trova un reseller

Sai già di cosa hai bisogno? Vorresti la comodità dell’acquisto e della spedizione online? Alcune categorie di prodotti Vertiv si possono acquistare tramite un reseller online.


Trova un reseller online

Hai bisogno di aiuto per scegliere un prodotto? Parla con un esperto di Vertiv altamente qualificato che ti orienterà verso la soluzione più adatta.



Contatta un esperto di Vertiv

The page you're viewing is for Italian (EMEA) region.

Modular data centers in federal tech for AI modernization

4 min. Lettura
Prefabricated modular data centers (PMDCs) are driving federal IT modernization and AI adoption, creating investment opportunities and responding to increasing demand in a rapidly growing market.

The U.S. government is accelerating its adoption of artificial intelligence (AI) and modern data infrastructure, creating a golden opportunity to invest, plan, and ride on the next wave of IT modernization. Prefabricated modular data centers (PMDCs) are emerging as the backbone of this transformation. By meeting federal IT and AI demands with unprecedented scalability, compliance, and speed, these modular solutions are not just an infrastructure innovation, but also a compelling investment opportunity.

Here’s why PMDCs are reshaping the federal landscape and how key decision makers and investors can reap the benefits of this rapidly growing sector.

The federal AI push drives demand for PMDCs

Outdated IT infrastructure and long procurement cycles limit agencies’ ability to deploy AI capabilities. Since 2020, federal agencies have been under pressure to keep pace with commercial AI innovation and national security requirements. The government has made it clear that AI is a national priority with legislation like the Federal Data Center Enhancement Act of 2023 and recent executive orders aimed at removing adoption barriers.

Enter PMDCs: These plug-and-play data center solutions are built off-site and deployed in months instead of the years required for traditional facilities. With the ability to handle advanced AI workloads, PMDCs are enabling federal agencies to modernize quickly and efficiently, creating a massive market for manufacturers, suppliers, and investors.

The market potential

The modular data center market is already experiencing significant growth, with analysts forecasting continued double-digit expansion. When tailored for federal use, PMDCs address unique operational, security, and compliance needs, unlocking a specialized segment in an already booming industry.

Key growth drivers include:

  • AI investment surge: Federal spending on generative AI is expected to jump by 35% in 2025, according to IT budget projections.
  • Environmental goals: Executive Order 14057 has outlined stringent environmental mandates, driving demand for energy-efficient data centers like PMDCs.
  • Technology refresh cycles: Unlike traditional data centers, which quickly become outdated, PMDCs offer built-in refreshes every 36 to 72 months, providing agencies can adopt the latest innovations.

11.3 years: Average age of a global data center.

Why PMDCs are a smart investment

For investors, this means a growing, stable market tied to both initial deployments and future updates.

Scalable solutions for expanding needs

Traditional data centers are often site-specific and require extensive upfront capital. PMDCs, on the other hand, offer modular scalability, enabling federal agencies to expand capacity incrementally as their needs grow. With configurations that stack vertically or sequence side-by-side, these centers maximize output while minimizing physical and financial waste. This scalability appeals to investors not only because it reduces upfront costs but also because it enables a broader customer base, from smaller agencies to large-scale federal deployments.

Compliance as a built-in feature

Federal contracts come with stringent regulatory requirements that can delay or derail infrastructure projects. PMDCs are pre-certified for critical standards like Federal Information Security Management Act (FISMA) and Federal Risk and Authorization Management Program (FedRAMP), drastically improving approval timelines and deployment speed. The ability to “bake in” compliance removes one of the most significant roadblocks in federal procurement, making PMDCs a safer and faster option for agencies while presenting lower-risk investment opportunities for stakeholders.

Environmental goals lead the way

Federal agencies are increasingly aligning with environmental responsibility and efficiency goals, and PMDCs deliver on this front. These modular solutions utilize energy-efficient cooling systems and smarter designs that reduce carbon footprints compared to traditional stick-built facilities. Options like Vertiv™ TimberMod™ even incorporate mass timber structures to further lower embodied carbon emissions.

Use cases highlight opportunities

The adaptability of PMDCs opens doors to diverse federal applications, further broadening market potential:

  • National security: Supporting sensitive operations through hardened structures and advanced cyber-resilient technologies.
  • Disaster response: Enabling mobile compute capabilities for FEMA and other emergency services.
  • Healthcare and civil services: Expanding AI-driven analytics for agencies like HHS and Veterans Affairs.

Each use case represents a potential investment and research niche, providing a diversified portfolio of opportunities under the broader federal umbrella.

The time to invest is now

The federal government is in the midst of its most ambitious push toward AI and IT modernization yet. PMDCs represent a low-risk, high-reward opportunity in a market with steady, long-term growth potential. With modular data centers sitting at the intersection of scalability, compliance, and innovative technology, multiple industries are perfectly poised to meet the moment. The white paper “Federal IT Modernization and AI Adoption with Modular Data Centers” presents deeper and more detailed insights and opportunities for key decision makers.

Download the white paper


Disponibilità e operatività Conformità e sicurezza Edge Efficienza Ottimizzazione della struttura Partners

VertivTM AI Hub

Un'infrastruttura progettata per supportare con anticipo più generazioni di piattaforme di calcolo, a partire da ORA.

Ulteriori informazioni
Login dei partner

Lingua & Ubicazione