Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv™ VR Rack Guaranteed Compatibility

 

Vertiv-VR-Rack-Guaranteed-Compatibility-WEB_309439_0.jpg

Vertiv™ VR Rack Guaranteed Compatibility

Vertiv guarantees that all EIA-310-E certified equipment will fit in to a Vertiv VR Cabinet.  If the equipment does not fit, Vertiv will return the End User’s money back. 

Background on EIA-310 Specification:

Adopted from the telecommunications industry, the 19” standard has been widely accepted in the IT market since inception.  The specification calls out the critical dimensions that are required for IT gear to safely mount in a cabinet. The critical dimensions can be seen below:

 

VR-Rack-Critical-Dimensions.png

Guaranteed Compatibility Eligibility:

  1. All Cabinet-Mount Equipment meets the 19” EIA Standard 310-E
  2. Vertiv VR Cabinet is the cabinet in question
  3. Vertiv is notified within 30 days of purchase that the equipment is not compatible
  4. The end user is able to send the cabinet in question back and can share the specification for the IT equipment being used
PORTALS

Language & Location