Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Introduces Vertiv™ DynaFlex Battery Energy Storage System, To Support Energy Grid Independence for Mission Critical Applications in North America and EMEA

November 09, 2023

Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the Vertiv™ DynaFlex BESS, a battery energy storage system designed to enable energy independence and bolster sustainability efforts at mission critical facilities. Available today in North America and EMEA, the Vertiv DynaFlex BESS provides flexibility in the use of utility power and is a critical step in the deployment of a dynamic power architecture. The system allows organizations to fully leverage the capabilities of hybrid power systems that include solar, wind, hydrogen fuel cells, and other forms of alternative energy. 

The lithium-ion batteries in the Vertiv DynaFlex BESS provide utility-scale energy for long duration support, allowing seamless and repeated transitions between energy sources. When paired with the optional Vertiv™ DynaFlex EMS (Energy Management System), the Vertiv DynaFlex BESS enables advanced energy management strategies, such as demand management and sharing or selling energy back to the grid that can result in a reduction of utility energy consumption and costs and potentially generate revenue for the parties involved. 

According to Omdia’s Market Landscape: Battery Energy Storage Systems report, “Enabling the battery ESS to interact with the smart electric grid is an innovative way of contributing to the grid through the balance of energy supply and demand, the integration of renewable energy resources into the power equation, the reduction or deferral of grid infrastructure investment, and the creation of new revenue streams for stakeholders.” 

“Sustainability has become a core tenet of many organizations’ growth plans, but concerns about operational resilience and growing stress on the grid have limited efforts to adopt alternative energy sources,” said Peter Panfil, vice president, global power, Vertiv. “The Vertiv™ DynaFlex BESS opens the full energy management toolbox. It allows organizations to leverage the strengths of these new energy generation assets and relegates the traditional utility provider to a complementary role in a more dynamic, efficient, and reliable mix of energy sources.” 

The Vertiv DynaFlex BESS is designed specifically for mission critical environments, such as commercial industrial facilities, high-value manufacturing plants, data centers, and other facilities where power plays a critical role. The system’s power conversion system (PCS) is designed to support 2 millisecond output, virtually eliminating any delays while shifting the load between hybrid power sources. Paired with an uninterruptible power supply (UPS) system, the reliable, highly efficient design of the Vertiv DynaFlex BESS reduces the risk of data center outages and diesel generator starts. 

The UL9540A-tested lithium-ion batteries in the Vertiv DynaFlex BESS are designed to minimize fire risks, are free-standing with a small footprint, and are designed for modularity. 

For more information on the Vertiv DynaFlex BESS and other innovative power solutions from Vertiv, visit Vertiv.com

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com. 

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise. 

CONTACT

Sara Steindorf
T +314-982-1725
E sara.steindorf@fleishman.com

Related Articles

PORTALS
Partner Login

Language & Location