Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

How Chilled Water Systems Meet Data Center Availability and Sustainability Goals

How Chilled Water Systems Meet Data Center Availability and Sustainability Goals

The data center industry continues to develop larger data centers to meet capacity demands, while at the same time taking steps to significantly reduce the impact of data centers on the environment. Cooling systems, and in particular, chilled water systems can play an important role in this evolution. They allow owners and operators to develop new data centers that are more efficient by addressing both direct and indirect emissions, which are factored into the total equivalent warming impact (TEWI) metric. The ability of a chilled water system to drive down both direct and indirect emissions allows critical facility operators to achieve a low TEWI. Chilled water systems also effectively balance water and energy usage for efficient cooling systems to support a low water usage effectiveness (WUE). The combination of low TEWI and low WUE makes chilled water systems one of the most sustainable choices for data center thermal management in terms of energy and water efficiency. These systems have been adapted to follow the evolution of data centers to non-raised floor designs and can help facilitate the transition to liquid cooling.

Today’s chilled water systems reduce direct emissions by limiting the amount of refrigerant used compared to other technologies and enabling the use of new, greener refrigerant types available in the market. These systems also reduce indirect emissions when they adopt new technologies and the system is optimized via best practices regarding system control, as described in this paper.

PORTALS

Language & Location