Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

As critical power requirements in today’s high availability data centers continue to increase, IT and facility managers are seeking greater power capacity along with superior reliability and energy efficiency.

Every business has unique needs for their data center. For those who deem maximum protection as their main concern, it is their top priority to specify an uninterruptible power supply (UPS) system designed to provide features that maintain quality power at all times. High availability data and network applications need to be supported by blade servers and high-density racks that demand increased power protection.

Large data centers generally use high capacity, centralized UPS systems to provide power protection for critical IT infrastructure. These systems incorporate the latest power protection technology to create a new level of reliability and efficiency. A data center UPS will usually be of the online double conversion type, the most reliable configuration, capable of handling a wide window of input conditions including power from backup generators—while still providing computer grade output to the critical load.

A UPS of this design is capable of supporting high power applications in medium to large data centers that are facing growing capacity demands. The ideal data center UPS will feature an optimized, industry leading footprint and power density, excellent operating efficiency and robust electrical protection to achieve superior cost savings.

IT professionals know how critical core data center capacity is to the success of their organizations. It’s where thousands of fundamental tasks happen every moment, and without it, productivity and profits are lost. The data center UPS is key to maintaining the operation of these critical IT functions.

Featured Products

PORTALS

Language & Location