Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

 

 

Background

Faced with growing demands for high-speed broadband services, the customer was looking at expanding the capacity of its upstream connection bandwidth with the international internet gateway. Increasing the bandwidth, however, means more power is required to support the new infrastructure.

During the design stage, the customer was met with a few challenges. First, the new server room is located at the building's second floor, making it difficult to use traditional 48V DC power equipment due to cabling concerns and possible high voltage drop as the power room is situated at the ground floor with some 50 meters from the server room. In addition, the server room space is small and has limited floor area for IT equipment.

 

Case Summary

Location:

Malaysia

Critical Need:

The customer was looking for a cost-effective, yet high-efficient power solution to support its capacity expansion, while addressing existing infrastructure challenges.

Vertiv Solution:

Netsure™ HVDC series

 

What is HVDC?

HVDC, or high-voltage direct current, utilises 240-400V DC energy to distribute power within a facility or data centre. Traditionally, a facility utilises power from a grid that is converted and distributed throughout the facility. However, in telecom or high-density applications, utilising energy from the grid can be inefficient due to multiple energy conversions that result in wasted energy. In this instance, DC power is the best alternative to optimise the unnecessary conversion steps thereby reducing the power losses.

DOWNLOAD THE CASE STUDY

PORTALS

Language & Location