The page you're viewing is for English (LATAM) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (LATAM) region.

Heat rejection cooling efficiency: Location, climate-based thermal management strategy

11 min. Read

As artificial intelligence (AI) and high-performance computing (HPC) push chip temperatures toward 40-45°C/104-113°F, a recurring theme has emerged: higher chip temperatures automatically enable compressor-less cooling. The reality is far more complex.

Download the white paper

This white paper reexamines conventional thinking by demonstrating that effective thermal management depends on three critical factors working together:

  • Chip operating temperature 
  • Local climate conditions, and 
  • Water availability. 

Through our comprehensive Air Cooling and Chilled Water Heat Rejection Maps, we reveal why a data center in Phoenix, in Dubai or Perth operating at 40°C/104°F still requires compressors as external ambient temperatures exceed the thermal differential needed for passive cooling, while a facility in Scandinavia or in Canada at the same working temperature can leverage compressor-less technology.

Key insights covered in this white paper include:

  • The climate reality: Over 90% of North American data centers are built in regions with design temperatures ≥40°C/104°F, severely limiting compressor-less adoption regardless of chip temperature increases.
  • Operational zones: A framework identifying which cooling technologies work best based on server temperature, ambient conditions, and water use. 
  • The water trade-off: How adiabatic systems and other solutions that rely on evaporative processes, such as cooling towers and hybrid coolers, can extend compressor-less viability, but introducing water consumption, cost, and regulatory challenges. 
  • Air cooling considerations: How optimal temperature differential (ΔT) of 10-12°C/50-54°F between return and supply air make a difference, the three operational zones for indoor water units when air cooling alone becomes less efficient, and how dedicated secondary water loops may be required in the long run. 
  • Location-specific strategies: Detailed climate zone mapping across North America, Europe, and Asia-Pacific showing where different cooling approaches make practical and economic sense. 

The strategic implications are clear: Operators need to re-evaluate their infrastructure and the geographic applicability of compressor-less technologies. Whether designing new facilities or retrofitting existing infrastructure, this paper provides the strategic rationale to match the right cooling technology to the data center’s operational environment.

Learn why the path to efficiency is not one-size-fits-all and discover which solutions align with your specific temperature, climate, and water constraints.

+

AI Artificial intelligence Colocation Consultants Data center innovation Efficiency ESG/sustainability ESG/Sustainability Extreme densification Facility Optimization Liquid Cooling Thermal chain evolution Thermal management Thermal Management Total Cost of Ownership Trends

VertivTM AI Hub

Infrastructure designed to stay multiple compute generations ahead, starting now.

Learn more
Partner Login

Language & Location