The page you're viewing is for English (LATAM) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (LATAM) region.

What AI processor architectures mean for data center infrastructure

11 min. Read

AI processor choices shape more than compute performance. They determine rack density, load behavior, cooling strategy, and the infrastructure model needed to turn available power into useful AI output.

AI compute is no longer a single architecture. Hyperscalers run custom Application-Specific Integrated Circuits (ASICs) alongside Graphics Processing Units (GPUs); enterprises deploy mixed CPU and GPU stacks, and inference workloads behave nothing like training. The processor you choose changes what your facility must deliver. Power density, cooling method, load profile, and deployment model all shift with the silicon.

For years, CPU workloads ran stable at 5–10KW per rack, and facilities were designed around that steady baseline. AI changed the equation. GPUs are 100x more efficient than CPUs for parallel AI workloads, producing more compute from the same amount of power. But AI demand is growing faster than efficiency gains, with AI chips requiring up to five times the power and five times the cooling capacity of a traditional server in the same space.

The infrastructure conversation has shifted accordingly, from counting installed megawatts to maximizing useful AI output with tokens per second per megawatt as a key supporting metric. This article examines how different AI processor architectures behave, what they demand from power and cooling systems, and how to match each architecture to the right infrastructure model.

What is the difference between CPU, GPU, TPU, and custom AI processor architectures?

AI workloads run on several types of processors, each designed for a different purpose. Understanding the role of each architecture is the first step in understanding its infrastructure requirements.

Central processing units (CPUs)

While GPUs, TPUs, and other accelerators perform most of the computationally intensive AI processing, CPUs manage the supporting functions that keep those workloads running, including data movement, memory management, storage access, networking, scheduling, and workload orchestration. For example, during AI training or inference, CPUs prepare and route data to accelerators, coordinate communication across systems, and manage the software environment that enables AI models to operate.

Graphics processing units (GPUs)

GPUs perform most of the computationally intensive processing required in AI training and inference, including large language and image-generation models, recommendation systems, and other deep learning applications. GPUs can scale from a few accelerators to thousands of interconnected processors working on the same model and can provide 20-50 times the compute power of a CPU for AI workloads.

Tensor processing units (TPUs)

TPUs are optimized specifically for the tensor operations that form the mathematical foundation of deep learning. Tensors are multidimensional arrays of data used to represent inputs, outputs, weights, and other values inside AI models. Designed by Google, TPUs accelerate these calculations to improve throughput and performance for large-scale AI training and inference.

Custom AI chips

Customization is the next step in the AI processor evolution. As organizations seek more performance and efficiency from demanding AI workloads, hyperscalers including Amazon Web Services, Microsoft Azure, Google Cloud, and Meta are developing processors tailored to their own AI ecosystems. Custom chips are designed to accelerate specific training and inference workloads while improving the amount of AI output generated from available power and infrastructure.

Traditional server (CPU only) vs AI server (CPU+GPU) to represent accelerated IT and HPC architectures illustration

Traditional server and AI server shown side by side to illustrate how accelerated IT and HPC architectures increase chip power consumption, heat generation, rack density, and the need for redesigned power and cooling infrastructure for AI workloads.

How do training and inference workloads create different infrastructure demands?

Training and inference place different stresses on data center infrastructure. Training creates long, sustained demand. Inference creates short, repeated bursts. Infrastructure has to support both patterns without assuming AI behaves like a steady enterprise IT load.

Training creates sustained high load

Training workloads run for long periods at high utilization as GPUs perform intensive iterative computations near maximum capacity. This creates a consistently heavy power draw rather than frequent idle-to-peak swings.

Inference creates fast, repeated power swings

Inference behaves differently because demand can jump from idle to full load in milliseconds. These bursts can exceed 150% of nominal power and repeat every few seconds. In practice, AI systems can move from roughly 10% utilization to full capacity at 100–150% almost instantaneously.

Dense AI racks magnify both load profiles

Because AI racks pack many GPUs or TPUs into a small footprint, those workload patterns translate into much higher infrastructure demand. AI racks can draw 30 kW to hundreds of kW per rack, compared with 5–10 kW for a typical enterprise IT rack. Traditional power infrastructure was not designed for this combination of high density and rapid fluctuation.

Infrastructure response to dynamic AI loads

Vertiv testing has shown that Vertiv™ Liebert® EXL S1, Vertiv™ Trinergy™, and Vertiv™ PowerUPS 9000 can handle AI load steps from 0% to 100% capacity without battery involvement when utility power remains within nominal parameters, while continuous fluctuations can be mitigated through testing and power-smoothing technology.

Why do AI processor architectures matter for data center infrastructure?

Rack density and facility scale start with processor architecture

Processor architecture determines how much compute can be packed into each rack, which in turn drives the facility design. Dense AI racks require coordinated choices across power distribution, heat rejection, white space, controls, and service access. The processor decision therefore becomes an infrastructure decision, not just an IT procurement choice.

Processor choices shape the electrical load profile

AI processors do not simply raise total demand; they change how demand behaves. Training can create sustained high utilization, while inference can create fast load swings. As AI scales, the infrastructure question is whether power delivery, UPS systems, rack PDUs, and controls can support high-density workloads without treating them like steady enterprise IT loads.

Higher densities demand new cooling strategies

AI processor choices affect how much power and heat each rack must support. Densities that once topped out at 35 kW have already climbed to 140 kW, with newer architectures pushing toward 240–250 kW per rack. In the near term, rack designs are expected to reach 300–600 kW, with some projections exceeding 1 MW by 2030.

Infrastructure must support successive processor generations

AI processor generations are moving quickly, and each generation changes the ratio of useful AI output to facility power. Efficiency gains can improve output per megawatt, but they do not remove the need for more power. AI demand continues to grow faster than chip efficiency, so total power used still rises. Facilities therefore need power and cooling systems that can scale across several compute generations, not a design locked to one processor family.

That is the infrastructure significance of AI processor architecture: each chip type creates a different electrical and thermal profile, and each generation changes the ratio of useful AI output to facility power. Operators that design power, cooling, and compute as one coordinated system will be better positioned to turn secured power into useful AI output while supporting multiple compute generations.

Watch how Vertiv integrates power, cooling, IT white space, services, and digital controls to support AI processor architectures at scale, from pilot deployments to high-density AI factories built for multiple compute generations.

What does ‘tokens per megawatt’ tell you about processor and infrastructure efficiency?

Facility power becomes measurable AI output

Tokens per megawatt measures useful inference throughput relative to a data center’s provisioned power budget. Because it accounts for all-in utility power, including power delivery and cooling overhead, it gives operators a more practical view of facility-level efficiency than chip thermal design power alone.

Power must translate to productive capacity

Power is the binding constraint for new AI deployments, so the planning question is shifting from how many megawatts are available to how much useful AI output those megawatts can produce. The market is moving from counting announced megawatts to maximizing the inference output generated from every contracted or self-generated electron, including revenue-generating inference tokens.

Workloads determine valid efficiency comparisons

Tokens per megawatt also helps compare how efficiently newer processors convert facility power into AI output when the workload conditions match. A 1 MW AI factory running the Hopper architecture generates 180,000 tokens per second at maximum volume. Blackwell delivers 10x throughput per megawatt for sparse mixture models compared with Hopper and lowers cost per million tokens 15x versus the prior generation. Across six GPU generations, inference throughput per megawatt has increased by 1,000,000x.

Tokens/MW is most useful when comparisons use the same model, workload shape, precision, and interactivity target. Otherwise, a high-throughput, low-interactivity result can look efficient while still failing the target user experience.

Infographic showing how tokens per megawatt is calculated

Infographic showing how tokens per megawatt is calculated by dividing useful inference tokens per second by provisioned utility power, helping compare how efficiently AI infrastructure turns available power into productive output.

How do hyperscale and enterprise infrastructure models differ for AI processors?

Hyperscale and enterprise AI infrastructure models differ because they optimize for different processor environments. Hyperscalers build dedicated, high-density AI factories around massive GPU or custom ASIC clusters. Enterprises more often integrate AI processors into mixed environments where flexibility, speed to deployment, governance, and cost predictability matter as much as raw scale.

Enterprises optimize for mixed workloads and deployment flexibility

Enterprise environments usually support mixed workloads and flexibility across CPUs, GPUs, and other accelerators. Rather than building fully custom AI factories, enterprises use standardized, commercially available systems configured for their sites. They may retrofit existing facilities, deploy a mix of GPUs, CPUs, and custom ASICs, or place workloads across public cloud, colocation, enterprise facilities, edge sites, and hybrid models, depending on data gravity, latency, governance, utilization, and business criticality.

Vertiv™ SmartIT for Enterprise addresses this enterprise segment by combining power, cooling, and rack infrastructure into a pre-validated package for 1–3 rack deployment models. It supports compute racks at 120–142 kW and is designed to maximize tokens per second per watt. The goal is faster operational readiness: moving AI from pilot to production, and from cost center to business value.

Enterprise environments often need hybrid cooling across mixed rack densities

Enterprise sites often need hybrid designs that support existing air-cooled equipment while preparing for liquid cooling. Most deployments combine direct liquid cooling for GPU racks with about a 20% air component, adding complexity across power distribution, cooling loops, and airflow. Vertiv collaborated with Intel to provide liquid- and air-cooled solutions for the Gaudi3 AI accelerator. The liquid-cooled solution has been tested at 160 kW accelerator power, and the air-cooled solution has been tested up to 40 kW of heat load.

Enterprises more often adapt existing electrical infrastructure

Enterprises more often adapt existing electrical architectures and use modular upgrades where possible. Vertiv™ PowerDirect provides up to 132 kW per rack for dense GPU environments, with integrated power telemetry and real-time load insights. Continuous-duty architectures such as the Vertiv™ Trinergy™ booster converter are built for extreme AI load swings. CPU workloads ran stable at 5–10 kW per rack, while GPU-driven racks can reach 140 kW. That jump changes the power train from a steady enterprise IT utility into a dynamic system that must manage volatile load steps from grid to chip.

Hyperscalers build around dedicated AI factories

Hyperscalers deploy AI processors at far larger scale, often in 1.5–100 megawatt AI factory chunks. These environments are designed around dense GPU or custom ASIC clusters, with power and cooling dedicated to the needs of those accelerators. Large-scale operators can justify custom-built IT systems, unique power train designs, and dense, GPU-powered facilities dedicated to AI workloads.

Hyperscale environments standardize around dense liquid-cooled clusters

Hyperscale AI factories are more likely to standardize around high-density liquid-cooled GPU or accelerator clusters. Current AI GPU designs are still mostly based on air cooling, but rising power use makes hybrid and liquid cooling more important. By the end of the decade, data centers are expected to rely heavily on liquid-cooling to the chip, self-contained immersion, and air cooling for residual heat loads. Liquid cooling is emerging as the primary response to GPU heat.

Hyperscalers can design dedicated power trains from grid to chip

Hyperscale environments can design power trains around dedicated AI clusters from grid to chip. AI platforms use GPUs that process thousands of operations simultaneously, creating sharp, short increases in demand. Distributing at higher voltages — 240V, 415V, or 480V rather than the traditional 208V — increases the power that can be delivered to racks and improves load balancing. With rack power needs rising, the rack PDU becomes more important for installation, protection against accidental disconnects, and cable management.

Hyperscale platforms favor large integrated infrastructure blocks

At AI factory scale, the core implication is that power, cooling, white space, and management tools must be designed together instead of as separate parts. Vertiv™ OneCore is a prefabricated AI-factory design built to operate as one system, from grid-level power delivery through chip-level thermal management. It delivers scalable blocks with densities configurable up to 600 kW per rack and can reduce on-site work, commissioning, and time-to-token by up to 50% compared to traditional builds.

Phased deployment supports enterprise, regional, and large-scale models

For deployments in the 3–10 MW range targeting enterprise AI clusters, regional colocation, or dedicated inference infrastructure, Bring Your Own Power and Cooling can compress deployment from years to months. For larger deployments of 100 MW and above, phased BYOP&C architectures support dynamic load responsiveness, thermal reuse, and scalability across multiple compute generations. The shared goal is to integrate the power train, thermal chain, IT white space, controls, and services without anchoring the architecture to a single compute ecosystem.

Next steps: match processor choices to infrastructure realities

Start with the workload

Matching AI processors to infrastructure starts with workload behavior, not chip preference. Identify whether the deployment is primarily training, inference, or mixed, and whether it creates sustained demand, rapid load swings, or both. Then define the processor environment: CPU-based mixed IT, dense GPU clusters, TPU or custom ASIC platforms, or a mixed accelerator estate.

Translate processor behavior into rack requirements

Next, calculate the rack-level requirements: power density, load behavior, heat rejection, cooling method, physical space, and controls. Dense accelerator racks may require liquid cooling and high-capacity rack power distribution, while mixed enterprise environments may need hybrid designs that support both existing IT and new AI accelerators.

Choose the deployment model that can scale

From there, select the infrastructure model that fits the workload and organization: an existing enterprise facility, a pre-integrated rack-level system, colocation or hybrid deployment, or a dedicated AI factory. The right model coordinates compute, power, cooling, white space, and controls while retaining enough flexibility to support the next generation of silicon.

Conclusion: design for useful AI output, not just installed capacity

The takeaway is simple: processor architecture determines workload behavior, and workload behavior determines infrastructure fit. Operators that plan for density, load volatility, cooling evolution, and processor refresh will be better positioned to convert available power into useful AI output.


Frequently asked questions

What is an AI processor architecture?

An AI processor architecture is the chip design used to run AI workloads, including CPUs, GPUs, TPUs, and custom AI chips.

Why do AI processors affect data center infrastructure?

AI processors change rack density, power draw, heat output, load behavior, and the cooling approach needed to support AI workloads.

How are CPUs, GPUs, TPUs, and custom AI chips different?

CPUs handle general computing, GPUs process parallel AI tasks, TPUs accelerate tensor operations, and custom chips are built for specific AI environments.

How do training and inference workloads differ?

Training creates sustained high load, while inference creates fast, repeated load swings as AI systems respond to user requests.

What does ‘tokens per megawatt’ mean?

Tokens per megawatt measures how much useful AI inference output a data center produces from its provisioned power budget.

Why is tokens per megawatt useful?

Using the tokens per megawatt formula helps operators judge whether available power is becoming productive AI capacity, not just installed megawatts.

Can tokens per megawatt compare processor generations?

Yes, tokens per megawatt can be used to compare processor generations but only when the same model, workload shape, precision, and interactivity target are used.

How do hyperscale and enterprise AI infrastructure models differ?

Hyperscalers build high-density AI factories, while enterprises often use mixed, modular, or hybrid infrastructure models.

What should organizations plan for first?

Start with workload behavior, then size the rack-level power, cooling, space, and controls required for the processor environment.


VertivTM AI Hub

Infrastructure designed to stay multiple compute generations ahead, starting now.

Learn more
Partner Login

Language & Location