The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

Beyond uptime: How industrial power disturbances disrupt production

6 min. Read

A power anomaly triggers a chain reaction that freezes production lines. Stopping the cascade starts with identifying what standard defences miss.

As power quality drops, control systems misread signals, sequences fall out of sync, and processes move into states that standard protection doesn't cover.  Even small electrical shifts carry operational impact, setting failure in motion before alerts fire. How far the disturbance spreads depends on whether anything contains it.

Industrial environments often require a different class of power protection than commercial applications. Solutions such as the Vertiv™ PowerUPS 6000 Industrial are designed to help maintain process continuity (see Figure 1). These units support critical control equipment through power disturbances to reduce the risks of electrical events escalating into production interruptions.

Figure 1. The Vertiv™ PowerUPS 6000 Industrial UPS system redefines versatility for C&I applications like manufacturing, transportation, logistics, cement, and oil and gas with a compact, single- or three-phase design (6–200 kVA). Source: Vertiv.

How a power disturbance becomes a production failure

Industrial systems share buses, feeders, and tightly linked process stages, allowing disturbances to travel across the network. At the control layer, degraded power causes programmable logic controllers (PLCs), drives, and sensors to misread signals and break sequence integrity before operators see an alarm. Automated responses can trigger shutdowns or improper resets, disrupting material flow. Interdependent process stages then stall, reducing throughput and increasing scrap.

Why industrial recovery outlasts the disturbance

In chemicals, food processing, and precision machining, a process interruption converts work in progress into unrecoverable scrap, with material, energy, and processing time lost in full. Production recovery runs well behind power restoration. Teams must clear safety interlocks, rebuild sequences, and resynchronise interdependent systems before operations can resume. Each step extends the outage, and rework, wasted inputs, and delivery penalties can accumulate well beyond the event itself.

Why dedicated industrial power protection matters

Power disturbances don't need to cause an outage to impact production. Voltage sags, electrical noise, and brief interruptions can disrupt control systems and lead to costly process interruptions. Industrial UPS systems help maintain control integrity by delivering conditioned power during these events. In demanding manufacturing environments, features such as IP42-rated protection support reliable operation in environments exposed to dust and moisture.

Protecting what's at stake

As process sensitivity rises and automation deepens, the impact of a power disturbance compounds at every layer — electrical, control, production, and commercial. The facilities that hold their position under those conditions are the ones that treat power protection as a production specification, not a facility utility.

The Vertiv™ PowerUPS 6000 stabilises power across control and production systems in environments exposed   to electrical variability and demanding operating conditions. Combining rugged industrial design with IP-42 rated protection, the UPS helps reduce disruption risk, maintain process continuity, and support reliable operation in facilities challenged by power disturbances, dust, humidity, and other environmental stresses.

Keep power disturbances off the production line

Protect critical loads, maintain control integrity, and help keep operations running through power events.

Contact Vertiv today.

Frequently asked questions


Power architecture transformation

VertivTM AI Hub

Infrastructure designed to stay multiple compute generations ahead, starting now.

Learn more
PORTALS
Partner Login

Language & Location