Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Vertiv Announces Highly Efficient Mid-Size Modular UPS for High-Density Applications in Asia

24/11/22

The new Vertiv™ Liebert® APM Plus is designed for reduced energy use and CO2 emissions

Singapore [November 24, 2022] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduces the new Vertiv™ Liebert® APM Plus, a high-density, modular, and transformer-free uninterruptible power supply (UPS) system that delivers up to 97% efficiency in double conversion mode, and up to 99% efficiency in eco-mode. Available from 50 to 500kW, the Liebert APM Plus is available today throughout Asia, including Australia and New Zealand, and India.

The Liebert APM Plus architecture is designed to optimize energy use and heat dissipation, minimizing the demand and consumption of data center air conditioning systems. The combination of these factors reduces CO2 emissions to a minimum, thus helping data centers to meet environmental compliance standards.

The Liebert APM Plus is an upgrade from the Liebert® APM models, and is ideal for mid-size to large data centers in the telecom, hyperscale and colocation spaces. The Liebert APM Plus features a slimmer body at 600 millimeters, 50% smaller than the previous model without compromising on efficiency. Its smaller footprint, achieved through ultra-high density power modules, makes it ideal for providing power availability to mission-critical applications.

With its built-in FlexPower™ technology, the Liebert APM Plus allows for simple, fast expansion of system capacity with its modular design. Each FlexPower™ module combines scalable power with independent controls to auto-regulate operation, enhancing overall availability.

The Liebert APM Plus features a, hot-swappable design of most of the critical links, supporting low Mean Time To Repair. The robust UPS  can also tolerate temperatures up to 50 degrees Celsius with auto-derating. The system also allows for intelligent monitoring options, compatible with the Vertiv™ Environet™ Alert and the Vertiv™ LIFE™ services.

“The Liebert® APM Plus design shows our commitment to providing our customers with solutions that address the changes of a rapidly growing digital ecosystem,” said Arunangshu Chattopadhyay, director of power product marketing and head of central technical support at Vertiv Asia. “With its flexible design and enhanced features, this UPS is ideal to support the availability needs of today’s customers. Additionally, the Liebert APM Plus’s small footprint makes it ideal for use in Vertiv™ integrated solutions such as  SmartRow™ and SmartAisle™, as well as the Liebert® APT power distribution system.”

Explore more of Vertiv’s UPS solutions at www.Vertiv.com.

 

# # #

 

 

 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 24,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

 

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

 

CONTACT
Katrina Tirante
T +6326203600 Ext 7666
E Katrina.Tirante@vertiv.com

 

Reinier Dungca
T +6326203600 Ext 7657
E Reinier.Dungca@vertiv.com

PORTALS
Overview
Partner Login

Language & Location