The page you're viewing is for Japanese (Japan) region.

Vertivの製造担当者と連携すると、複雑な設計をお客様独自のニーズに合わせて構成することが可能になります。大規模なプロジェクトに関する技術的ガイドが必要な組織に対して、Vertivは十分なサポートを提供いたします。

詳細を見る

Vertiv再販業者パートナーと連携して、多くのお客様がITアプリケーション用のVertiv製品を購入しています。パートナーは、広範なトレーニングと経験を積み、ITおよびインフラに関するソリューション全体をVertiv製品で明確にし、販売、サポートを行うという独自の立場を構築しています。

再販業者を見つける

ご自身に必要なものについて特定済みですか? 便利なオンラインショッピングおよび配送をご希望ですか? 特定のカテゴリーのVertiv製品は、オンライン再販業者を通じて購入可能です。


販売代理店のECサイトを検索

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

The page you're viewing is for Japanese (Japan) region.

Designing liquid cooling infrastructure for scalability: Best practices for future growth

5 分 読む

From fluid network architecture to component sizing and expansion provisions, learn how data center operators can build infrastructure that grows with their facility’s needs.

Whether operators are looking to deploy liquid-cooled racks today, running a pilot program before a full production rollout, or planning ahead for business growth that will demand additional capacity, designing for scalability from day one prevents costly retrofits and operational disruptions down the road. The difference between a scalable liquid-cooling deployment and one that becomes a constraint lies in the initial design decisions regarding fluid network architecture, component sizing, and expansion provisions. Here's how to build infrastructure that grows with your needs.

Right-sizing your secondary fluid network

The secondary fluid network (SFN), the distribution system between your coolant distribution units (CDUs) and server racks, is where scalability often succeeds or fails. The key is understanding not just your current cooling load, but your realistic expansion trajectory.

Header sizing considerations

When specifying row-manifold headers, conventional wisdom suggests matching pipe diameter to current rack density. This approach creates problems quickly. A 4-inch header might serve the existing deployment today, but what happens when you need to add eight more racks to that row next year and the total capacity doubles?

A best practice calls for oversizing headers based on maximum anticipated row density. If you're deploying 100 kW racks today but know 200-300 kW configurations are coming, or if you're filling half a row initially with plans to complete it within 36 months, specifying properly sized headers from the start would be considered a best practice. The incremental cost of larger piping during initial construction is minimal compared to the expense and downtime of replacing undersized infrastructure later.

The same principle applies to branch connections. Even if you're initially deploying 1.5-inch connections to racks, design your header to accommodate up to 3-inch ports. This forward-thinking mindset allows you to upgrade individual racks to higher cooling capacities without reworking the entire distribution system.

Pressure drop and flow planning

Hydraulic calculations should assume full row utilization, not current deployment. Work backward from your maximum anticipated heat load per rack, calculate total flow requirements, and verify that pressure drop across the entire secondary network remains within acceptable ranges at peak capacity. This approach establishes that adding racks doesn't compromise cooling performance for existing equipment.

CDU capacity planning and redundancy

CDUs act as the connection point between facility infrastructure and IT loads. Proper CDU planning enables expansion without disruption.

Capacity headroom

A common mistake is sizing CDUs up to 90% utilization for initial deployments. While this maximizes equipment efficiency, it leaves no room for growth. Instead, target from 60% to 70% utilization during initial deployment. This allocation allows operators to add racks incrementally without requiring additional CDU capacity immediately.

When expansion does necessitate additional CDUs, modular infrastructure design becomes critical. Your facility loop should include pre-stubbed connection points for future CDU locations. These provisions, installed during initial construction, enable new CDUs to be integrated with minimal disruption to the facility.

Redundancy considerations for expansion

Redundancy architecture must account for future capacity, not just current loads. If you're operating two CDUs in an N+1 configuration today, adding significant rack capacity might require a third CDU to maintain redundancy. Plan your mechanical room layout and facility loop capacity with this expansion in mind.

Modular design enables faster expansion

The shift from custom-fabricated piping to modular, pre-engineered components has transformed liquid cooling scalability. Understanding the advantages of modular design helps optimize your deployment strategy.

Standardized connection points

Modular manifold systems feature consistent, repeatable connection interfaces. Sanitary tri-clamp fittings, for example, allow new manifold sections to be added without welding or specialized contractors. This standardization means expansion projects that once required weeks of downtime can now be completed in days.

When specifying your initial deployment, verify that all manifold modules use consistent connection standards. Mixing connection types between phases creates unnecessary complexity during future expansions.

Prefabricated frame systems

Modern manifold systems arrive as complete assemblies: headers, branches, frames, drip pans, and support structures integrated and tested before shipping. This prefabricated approach offers several scalability advantages. Installation time drops dramatically compared to field-fabricated piping. Quality control happens in controlled manufacturing environments rather than on-site. Testing and commissioning procedures are streamlined. Most importantly, expansion sections can be installed during brief maintenance windows rather than requiring extended facility shutdowns.

Quick-disconnect technology

Branch connections featuring quick-disconnect fittings enable rack-level changes without draining entire manifold sections. This capability is essential when incrementally adding racks to partially populated rows. New servers can be integrated while adjacent equipment continues operating normally.

Isolation strategies during expansion

The ability to expand capacity without impacting production workloads separates well-designed systems from problematic ones. Strategic isolation capabilities are essential.

Segment-level isolation

Design your SFN with isolation valves at logical boundaries. Each row manifold should have supply-and-return isolation capability at each rack position. Within large systems, consider additional isolation points that allow sections to be taken offline independently. This segmentation means when personnel add capacity or perform maintenance in one area, facility operators aren't required to shut down unrelated systems.

Testing and commissioning new sections

Before integrating new manifold sections with production infrastructure, complete thorough testing in isolation. This includes pressure testing to verify integrity, flushing procedures to remove contaminants, flow verification to confirm hydraulic performance, and leak detection with fluid quality verification. Only after new sections pass commissioning should they be connected to active systems. This discipline prevents construction debris or installation issues from contaminating established fluid networks.

Transitioning from air to liquid: A phased approach

Many facilities begin liquid cooling journeys by converting select high-density racks while maintaining air cooling elsewhere. This hybrid approach requires careful planning.

Install oversized facility loop capacity and CDU provisions even if initial liquid-cooled rack counts are small. The headway made in infrastructure investment enables future conversion of additional racks without revisiting mechanical systems. Design your row manifolds with blanked connection points for future racks, allowing air-cooled positions to convert to liquid cooling as refresh cycles occur.

Learning from pilot deployments

Pilot programs offer valuable operational experience before full-scale rollout. Design pilots with production scalability in mind. Use the same modular components, connection standards, and design approaches employed facility-wide. This facilitates the translation of lessons learned directly into larger deployments without requiring different infrastructure approaches.

Building for tomorrow's density

Data center cooling requirements aren't static. Processor roadmaps point toward continued density increases. Business growth drives rack count expansion. Designing liquid-cooling infrastructure with scalability provisions is essential to avoid premature obsolescence and maximize the value of infrastructure investments.

Ready to design a scalable liquid cooling deployment? Learn more about our high-density thermal management solutions here and contact our representatives on how we can support your plans and deployments from grid to chip.


AI 人工知能 Availability & uptime データセンターのイノベーション Efficiency Liquid Cooling サーマルチェーンの進化 Thermal management Total Cost of Ownership
Partner Login

言語と地域