The page you're viewing is for Italian (EMEA) region.

Rivolgiti a un rappresentante di Vertiv che lavorerà al tuo fianco e ti aiuterà a realizzare progetti complessi in base alle tue esigenze. Se la tua organizzazione ha bisogno di assistenza tecnica per un grande progetto, Vertiv può fornirti tutto il supporto necessario.

Ulteriori informazioni

Molti clienti si affidano ai reseller che sono partner di Vertiv per l’acquisto di prodotti ideali per le loro applicazioni IT. Affidati alle elevate competenze dei nostri partner che, grazie ai prodotti Vertiv, sono in grado di offrire soluzioni complete per infrastrutture e applicazioni IT: dalle specifiche alla vendita all’assistenza.

Trova un reseller

Sai già di cosa hai bisogno? Vorresti la comodità dell’acquisto e della spedizione online? Alcune categorie di prodotti Vertiv si possono acquistare tramite un reseller online.


Trova un reseller online

Hai bisogno di aiuto per scegliere un prodotto? Parla con un esperto di Vertiv altamente qualificato che ti orienterà verso la soluzione più adatta.



Contatta un esperto di Vertiv

The page you're viewing is for Italian (EMEA) region.

Peak edge performance

Edge is an evolution, not a revolution

Your customers are being asked to meet the ever-increasing demands of their business and downtime is not an option. They need confidence that their infrastructure will stay running well into the future, here are some ways you can help:

 

Downtime Cause Selling Tips: Solutions that can help:
Working with outdated technology

Ensure each critical path is set up with a redundant path so that if one device is turned off or fails, there is another that can step in its place.

Color coding receptacles or power cords to identify A/B feeds can help reduce the chance of accidental removal of cables.

Vertiv Geist rPDU

Vertiv Geist UPDU

Trellis Power Insight

Cyber Attacks You can help by ensuring the hardware purchased is set up with protection as well.

Data Security

Equipment Failure

Ensure proper backup power is purchased in case of a power outage

Liebert GXT5 UPS, 5-20 kVA

Liebert GXT5 UPS, 750-3000 VA

Ensure each critical path is set up with a redundant path so that if one device is turned off or fails, there is another that can step in its place.

Vertiv Geist rPDU

Vertiv Geist UPDU

Outdated equipment can put your customers at a greater risk for failure. Look for programs that help with the transition process.

Trade-In Program

Software Failure

Outdated software is more susceptible to security breaches.

Recommend a new solution that has proper security protocols. Software failure can happen when proper testing has not been done. Recommend to your customer to experiment and test the software before implementing.

Avocent ACS 800

ACS 8000

Avocent Local Rack Access Console

Natural Disasters

If in an area that is earthquake-prone OSHPOD certification is most likely required, Ensure proper backup power is purchased in case of a power outage.

Redundancy is key if your customer’s equipment is located in a high risk area for natural disasters. If possible – recommend setting up geo-redundancy (redundancy between physical locations).

Vertiv VR Rack

Liebert GXT5 UPS, 5-20 kVA

Liebert GXT5 UPS, 750-3000 VA

 

Helpful Talking Points

 

  • Though not every business is the same, a survey showed quarter of companies lose between $301,000-$400,000 per hour of downtime with another 14% losing more than five million dollars per hour.
  • The steep cost of outages not only imposes a direct financial effect, but an indirect operational one as well. The operational strain downtime puts on a business effects added labor and reduced productivity in most cases.
  • There is also an element of reputation loss depending on the company. Take Target’s major data breach in 2013/ That reportedly cost them $162 million, and effected more than 70 million customers, with many of them taking to social media.

Need more information?   Visit our Partner Portal

Perfeziona il loro Edge con l’infrastruttura Vertiv


Le attività dei tuoi clienti si affidano all’IT per supportare nuove applicazioni Edge e per migrare il computing e l’archiviazione più vicino a clienti, dipendenti e dispositivi. Tuttavia essi non possono fare tutto questo da soli.

In qualità di Architects of Continuity, Vertiv offre un ampio portfolio di sistemi di infrastrutture intelligenti, software e servizi in grado di affrontare le sfide di affidabilità, scalabilità e gestione che i tuoi clienti devono affrontare durante l’evoluzione di edge. Non importa quale sia la sfida, Vertiv ha la soluzione.

Per ulteriori informazioni, clicca sugli indicatori arancioni all’interno dell’immagine.

Gestione dell’hardware

Scopri come ridurre i tempi di inattività e migliorare la sicurezza del data center utilizzando l’accesso e il controllo da remoto di Avocent

Avocent ACS 800 Serial Console

Avocent ACS 8000 Advanced Console Server

Avocent Local Rack Access Console

Avocent MergePoint Unity KVM Switches

Avocent AutoView Series KVM

Avocent DSView Management Software

Rack & Enclosure

Prodotti rack e di contenimento flessibili ed economici per data center.

Vertiv VR Rack

Thermal Management

La base della gestione del flusso dell’aria nel data center è il design del corridoio caldo-freddo, nel quale gli armadi sono disposti in file alternate con prese d’aria (corridoi freddi) e scarichi d’aria (corridoi caldi) l’una di fronte all’altro. Questa configurazione consente agli operatori del data center di concentrare la portata d’aria di raffreddamento solo dove è necessario, nelle prese d’aria IT, e di evitare costi e inefficienze inutili derivanti dal condizionamento dell’intero spazio.

Sistema di condizionamento da rack Vertiv VRC fino a 3500 W

Sistema di condizionamento infrarack Vertiv VRC fino a 33kW

Monitoraggio remoto

Che si tratti di monitoraggio delle batterie, di sistemi di rilevamento delle perdite, della temperatura, dei sensori per ambienti industriali difficili o di altri sistemi complessi dei data center, siamo tutti concordi sul fatto che si tratta di una parte essenziale per la protezione e la sicurezza di un impianto critico.

Vertiv Environet Alert - Presto disponibile

Trellis Power Insight - Presto disponibile

UPS

UPS intelligente ed efficiente per la protezione delle tue applicazioni mission-critical

UPS Liebert GXT5, 5-20 kVA

UPS Liebert GXT5, 750-3.000 VA

Vertiv Liebert GXT RT+ Online 1.000-3.000 VA

Vertiv EDGE Line Interactive 500-3.000 VA

Distribuzione dell’alimentazione in rack

La linea di Rack PDU di Vertiv soddisfa i vari requisiti di distribuzione dell’alimentazione delle applicazioni IT e ambientali.​

Vertiv Geist rPDU

Vertiv Geist UPDU

Accesso e controllo da remoto Rack & Enclosure Condizionamento per rack Monitoraggio remoto UPS monofase Distribuzione dell’alimentazione in rack

Mark Your Calendars

Keep your edge by attending our upcoming events designed for our partners.

 

Articoli correlati a Edge

VR Rack Image Alt Text
Case Study

Infocrossing Manages Its Dynamic Data Centers with Feature-Rich V...

febbraio 18, 2020 Scopri di più
Login dei partner

Lingua & Ubicazione