The page you're viewing is for Italian (EMEA) region.

Rivolgiti a un rappresentante di Vertiv che lavorerà al tuo fianco e ti aiuterà a realizzare progetti complessi in base alle tue esigenze. Se la tua organizzazione ha bisogno di assistenza tecnica per un grande progetto, Vertiv può fornirti tutto il supporto necessario.

Ulteriori informazioni

Molti clienti si affidano ai reseller che sono partner di Vertiv per l’acquisto di prodotti ideali per le loro applicazioni IT. Affidati alle elevate competenze dei nostri partner che, grazie ai prodotti Vertiv, sono in grado di offrire soluzioni complete per infrastrutture e applicazioni IT: dalle specifiche alla vendita all’assistenza.

Trova un reseller

Sai già di cosa hai bisogno? Vorresti la comodità dell’acquisto e della spedizione online? Alcune categorie di prodotti Vertiv si possono acquistare tramite un reseller online.


Trova un reseller online

Hai bisogno di aiuto per scegliere un prodotto? Parla con un esperto di Vertiv altamente qualificato che ti orienterà verso la soluzione più adatta.



Contatta un esperto di Vertiv

The page you're viewing is for Italian (EMEA) region.

Expand as they need to

Edge is an evolution, not a revolution

Adding a couple of racks to scaling to new locations across the world, your customers are planning their next Edge deployments now. They need IT infrastructure that can keep up as their business grows. No matter how your customer is looking to scale, here are some tips for helping them through the process:

 

Their Edge Challenges: Selling Tips: Solutions that can help:

Limited space for expansion

Maximize usable space by recommending racks that will fit as much equipment as they can fit.

VR Rack – 42U, 45U and 48U

Recommend rack PDUsthat can handle more capacity than is needed today to allow for powering additional equipment in the future.

Vertiv Geist rPDU

Vertiv Geist UPDU

Rapidly expanding locations

Recommend products that have a reliable reputation and can be quickly shipped and installed.

Vertiv VR Rack

Liebert GXT5 UPS, 5 -20 kVA

Liebert GXT5 UPS, 750-3000 VA

Vertiv Geist rPDU

Vertiv Geist UPDU

Consider integrated solutions to take some of the installation headaches

Pre-integrated VR Racks

Look for products that reduce the total cost of ownership (TCO)

Liebert GXT5 UPS, 5 -20 kVA

Liebert GXT5 UPS, 750-3000 VA

Scaling quickly with limited on-site resources

Find a remote monitoring & management solution that allows them to not only view data but set alarms and make changes while not physically being there.

Avocent ACS 800

ACS 8000

Avocent Local Rack Access Console

 

Helpful Talking Points

 

Find a remote monitoring & management solution that allows them to not only view data but set alarms and make changes while not physically being there.

  

600x600-297954-Whats-Your-Edge-Scalability_299622_0.jpg

600x600-236523-whatsyouredge-scalability_299621_0.jpg

Here are some ways your customers are planning for expected growth now:

  • Efficiently adding compute capacity in new locations
  • Choosing site locations strategically
  • Tailoring availability to service requirements
  • Mitigating higher energy consumption with economization
  • Ensuring infrastructure scalability while minimizing capex
  • Enabling remote management

Need more information?   Visit our Partner Portal

Perfeziona il loro Edge con l’infrastruttura Vertiv


Le attività dei tuoi clienti si affidano all’IT per supportare nuove applicazioni Edge e per migrare il computing e l’archiviazione più vicino a clienti, dipendenti e dispositivi. Tuttavia essi non possono fare tutto questo da soli.

In qualità di Architects of Continuity, Vertiv offre un ampio portfolio di sistemi di infrastrutture intelligenti, software e servizi in grado di affrontare le sfide di affidabilità, scalabilità e gestione che i tuoi clienti devono affrontare durante l’evoluzione di edge. Non importa quale sia la sfida, Vertiv ha la soluzione.

Per ulteriori informazioni, clicca sugli indicatori arancioni all’interno dell’immagine.

Gestione dell’hardware

Scopri come ridurre i tempi di inattività e migliorare la sicurezza del data center utilizzando l’accesso e il controllo da remoto di Avocent

Avocent ACS 800 Serial Console

Avocent ACS 8000 Advanced Console Server

Avocent Local Rack Access Console

Avocent MergePoint Unity KVM Switches

Avocent AutoView Series KVM

Avocent DSView Management Software

Rack & Enclosure

Prodotti rack e di contenimento flessibili ed economici per data center.

Vertiv VR Rack

Thermal Management

La base della gestione del flusso dell’aria nel data center è il design del corridoio caldo-freddo, nel quale gli armadi sono disposti in file alternate con prese d’aria (corridoi freddi) e scarichi d’aria (corridoi caldi) l’una di fronte all’altro. Questa configurazione consente agli operatori del data center di concentrare la portata d’aria di raffreddamento solo dove è necessario, nelle prese d’aria IT, e di evitare costi e inefficienze inutili derivanti dal condizionamento dell’intero spazio.

Sistema di condizionamento da rack Vertiv VRC fino a 3500 W

Sistema di condizionamento infrarack Vertiv VRC fino a 33kW

Monitoraggio remoto

Che si tratti di monitoraggio delle batterie, di sistemi di rilevamento delle perdite, della temperatura, dei sensori per ambienti industriali difficili o di altri sistemi complessi dei data center, siamo tutti concordi sul fatto che si tratta di una parte essenziale per la protezione e la sicurezza di un impianto critico.

Vertiv Environet Alert - Presto disponibile

Trellis Power Insight - Presto disponibile

UPS

UPS intelligente ed efficiente per la protezione delle tue applicazioni mission-critical

UPS Liebert GXT5, 5-20 kVA

UPS Liebert GXT5, 750-3.000 VA

Vertiv Liebert GXT RT+ Online 1.000-3.000 VA

Vertiv EDGE Line Interactive 500-3.000 VA

Distribuzione dell’alimentazione in rack

La linea di Rack PDU di Vertiv soddisfa i vari requisiti di distribuzione dell’alimentazione delle applicazioni IT e ambientali.​

Vertiv Geist rPDU

Vertiv Geist UPDU

Accesso e controllo da remoto Rack & Enclosure Condizionamento per rack Monitoraggio remoto UPS monofase Distribuzione dell’alimentazione in rack

Mark Your Calendars

Keep your edge by attending our upcoming events designed for our partners.

 

Articoli correlati a Edge

VR Rack Image Alt Text
Case Study

Infocrossing Manages Its Dynamic Data Centers with Feature-Rich V...

febbraio 18, 2020 Scopri di più
Login dei partner

Lingua & Ubicazione