The page you're viewing is for Spanish (LATAM) region.

Al trabajar con el soporte de ventas de Vertiv, puede configurar los complejos diseños de acuerdo con sus necesidades específicas. Si forma parte de una organización que busca orientación técnica para un proyecto grande, Vertiv puede ofrecerle el soporte que necesita.

Más información

Muchos clientes trabajan con un socio revendedor de Vertiv para comprar productos de Vertiv para sus aplicaciones de TI. Los socios cuentan con amplia capacitación y experiencia, y están en una posición única para especificar, vender y brindar soporte a soluciones completas de TI e infraestructura con los productos de Vertiv.

Buscar un revendedor

¿Ya sabe lo que necesita? ¿Desea la comodidad de comprar y enviar en línea? Ciertas categorías de productos de Vertiv se pueden comprar a través de un revendedor en línea.


Encontrar un vendedor en línea

¿Necesita ayuda para elegir un producto? Hable con un especialista de Vertiv altamente calificado, quien le guiará hacia la solución adecuada para usted.



Contactar a un especialista de Vertiv

The page you're viewing is for Spanish (LATAM) region.

Heat rejection cooling efficiency: Location, climate-based thermal management strategy

10 min. Leer

As artificial intelligence (AI) and high-performance computing (HPC) push chip temperatures toward 40-45°C/104-113°F, a recurring theme has emerged: higher chip temperatures automatically enable compressor-less cooling. The reality is far more complex.

Download the white paper

This white paper reexamines conventional thinking by demonstrating that effective thermal management depends on three critical factors working together:

  • Chip operating temperature 
  • Local climate conditions, and 
  • Water availability. 

Through our comprehensive Air Cooling and Chilled Water Heat Rejection Maps, we reveal why a data center in Phoenix, in Dubai or Perth operating at 40°C/104°F still requires compressors as external ambient temperatures exceed the thermal differential needed for passive cooling, while a facility in Scandinavia or in Canada at the same working temperature can leverage compressor-less technology.

Key insights covered in this white paper include:

  • The climate reality: Over 90% of North American data centers are built in regions with design temperatures ≥40°C/104°F, severely limiting compressor-less adoption regardless of chip temperature increases.
  • Operational zones: A framework identifying which cooling technologies work best based on server temperature, ambient conditions, and water use. 
  • The water trade-off: How adiabatic systems and other solutions that rely on evaporative processes, such as cooling towers and hybrid coolers, can extend compressor-less viability, but introducing water consumption, cost, and regulatory challenges. 
  • Air cooling considerations: How optimal temperature differential (ΔT) of 10-12°C/50-54°F between return and supply air make a difference, the three operational zones for indoor water units when air cooling alone becomes less efficient, and how dedicated secondary water loops may be required in the long run. 
  • Location-specific strategies: Detailed climate zone mapping across North America, Europe, and Asia-Pacific showing where different cooling approaches make practical and economic sense. 

The strategic implications are clear: Operators need to re-evaluate their infrastructure and the geographic applicability of compressor-less technologies. Whether designing new facilities or retrofitting existing infrastructure, this paper provides the strategic rationale to match the right cooling technology to the data center’s operational environment.

Learn why the path to efficiency is not one-size-fits-all and discover which solutions align with your specific temperature, climate, and water constraints.

+

AI Inteligencia artificial Coubicaciones Consultants Innovación del centro de datos Eficiencia ESG/SOSTENIBILIDAD ESG/SOSTENIBILIDAD Densificación extrema Optimización de instalaciones Liquid Cooling Evolución de la cadena térmica Gerenciamiento térmico Gerenciamiento térmico Costo total de propiedad Trends

Centro de IA VertivTM

Infraestructura diseñada para mantenerse por delante de múltiples generaciones de computación, a partir de ahora.

Más información
PRODUCTOS Y SERVICIOS
Descripción general
Iniciar Sesion Como Socio

Idioma y ubicación