The page you're viewing is for Spanish (LATAM) region.

Al trabajar con el soporte de ventas de Vertiv, puede configurar los complejos diseños de acuerdo con sus necesidades específicas. Si forma parte de una organización que busca orientación técnica para un proyecto grande, Vertiv puede ofrecerle el soporte que necesita.

Más información

Muchos clientes trabajan con un socio revendedor de Vertiv para comprar productos de Vertiv para sus aplicaciones de TI. Los socios cuentan con amplia capacitación y experiencia, y están en una posición única para especificar, vender y brindar soporte a soluciones completas de TI e infraestructura con los productos de Vertiv.

Buscar un revendedor

¿Ya sabe lo que necesita? ¿Desea la comodidad de comprar y enviar en línea? Ciertas categorías de productos de Vertiv se pueden comprar a través de un revendedor en línea.


Encontrar un vendedor en línea

¿Necesita ayuda para elegir un producto? Hable con un especialista de Vertiv altamente calificado, quien le guiará hacia la solución adecuada para usted.



Contactar a un especialista de Vertiv

The page you're viewing is for Spanish (LATAM) region.

Validating AI Factory design challenges with physical system-level testing

2 min. Leer

AI factory economics at scale depend on validated systems instead of individual components. Learn why infrastructure must be simulated and tested as an interdependent whole before deployment.

Download the app brief

AI factories are rewriting the economics of compute infrastructure at scale. Billions in capital committed against a single operational question: can electrical capacity be converted into productive compute quickly, reliably, and at a cost structure that justifies the investment?

The answer depends on how the complete physical system behaves as a convergent whole under real-world AI workload conditions. Namely, the power trains, thermal chains, controls, software, and the interfaces between them, working in sync.

Five intensifying forces are driving this shift:

  • Density is compressing the margin for error at the rack level.
  • Speed is making time to productive capacity the defining competitive metric.
  • Scale is turning manageable interactions into dominant engineering challenges.
  • Complexity is multiplying the interfaces where design intent diverges from physical reality.
  • Dynamic workload profiles are rendering steady-state assumptions obsolete.

The traditional validation approaches of testing individual components against isolated specifications remain necessary. However, they no longer address the question operators are asking on the ground: does the system work when everything runs simultaneously?

The gaps that matter most exist at the interfaces and seams between systems.

This application brief introduces a closed-loop validation methodology that connects virtual simulation, physical systems-level testing, field deployment, and operational learning into a continuous cycle. Each iteration reduces the variance between what was designed and what is delivered.

Figure 1. The closed loop enables the continuous reduction of variance between design intent and physical and operational reality. Source: Vertiv.

It examines how decades of distributed critical infrastructure validation capability can be consolidated and focused specifically for AI factory systems: validating combined power, thermal, and control behavior at greater scale, speed, and fidelity. And it frames the economic argument around four metrics that connect infrastructure performance to AI factory outcomes.

The brief provides a capacity validation framework; the questions to ask at each phase of the lifecycle, the indicators that distinguish validated confidence from inherited assumption, and the engineering logic behind treating infrastructure as a system rather than a collection of parts.

The infrastructure either performs as a validated system or performs as an assumption. AI factory economics leave increasingly little room for the latter.


AI All Services Inteligencia artificial Disponibilidad y funcionamiento Computación en nube Coubicaciones Potencia Crítica Innovación del centro de datos Diseño centrado en lo digital Edge Eficiencia Densificación extrema Optimización de instalaciones Campus a escala de gigavatios Liquid Cooling Maintenance Testing Monitoreo Transformación de la arquitectura de alimentación Services Infraestructura unificada
PRODUCTOS Y SERVICIOS
Descripción general
Iniciar Sesion Como Socio

Idioma y ubicación