Discover how six AI archetypes map workload demands to proven infrastructure designs
Vertiv presents a decision framework with six AI archetypes mapping workload demands to infrastructure and reference designs.
800 VDC architecture selection for high-density AI compute
As the AI era continues to progress and demand increases, conventional AC distribution is running out of physical space for conductors, connectors, and cooling infrastructure. 800 VDC offers a path forward. Operators can use this paper’s framework to evaluate each decision criteria and design element every deployment must address.
Power MW-scale racks: 800 VDC architectures for high-density AI compute
AI rack densities are approaching MW scale by 2027. Explore three 800 VDC distribution architectures (rack, pod, and facility-level) for next-generation data centers.
Inteligencia artificial
From pilot to production: Three enterprise AI infrastructure decisions that matter
Explore three enterprise AI infrastructure decisions that matter when moving from pilot to production: workload placement, token economics, and GPU-ready operations.
AI infrastructure moves from ambition to execution: Five conversations at DCD AI Week
Vertiv leaders join NVIDIA ecosystem partners, infrastructure experts, and industry researchers across five DCD webcasts examining how operators can turn AI ambition into deployable, productive, and adaptable capacity.
DCD AI Week 2026: From planning and design to deployment reality - What operators must solve next
Discover how AI infrastructure demands system-level design, from power train to thermal chain, in the first episode of DCD AI Week 2026.
Densificación extrema
Extreme densification: The defining macro force shaping data center design
Vertiv Frontiers: Extreme densification is a critical driver of modern data centers, accelerated by AI and HPC workloads, and creates additional complexity in power, cooling, and space.
Validating AI Factory design challenges with physical system-level testing
The gaps that determine whether AI factory capital produces productive compute exist at the seams between systems. This brief introduces the closed-loop validation methodology connecting simulation, physical testing, and operational learning into a continuous cycle of reduced uncertainty.
Spotlight: Bringing NVIDIA AI Computing Capability to the Naval Postgraduate School
Discover how Vertiv helped the Naval Postgraduate School deploy a high-density, liquid-cooled AI infrastructure powered by NVIDIA DGX GB300 to accelerate AI research, education, and mission-critical innovation.
Autonomía de la energía
BYOP implementation: Integrated planning for data center generation at scale
Learn five critical success factors for BYOP data center implementation.
Bring Your Own Power & Cooling (BYOP&C): An integrated approach to accelerate grid-to-chip deployment
AI workloads are driving rack densities into the triple digits and stretching interconnection queues beyond five years, creating stranded capacity and hidden capital costs. Traditional project‑build models can’t keep pace, leaving data centers stalled and delaying time‑to‑revenue.
Grid or on-site? The AI infrastructure decision
Grid or on-site? We explore the infrastructure decision shaping AI data center deployment — and why the five-year interconnection queue is forcing operators to choose.
Punto destacado de la serie de blogs
Innovar en voz alta
Para prosperar en los negocios, los empleados deben trabajar en conjunto y encontrar una manera de hacer cosas nuevas o mejorar las ya existentes, y luego asegurarse de que este proceso forme parte de la cultura de la compañía.
DCD AI Week 2026: From planning and design to deployment reality - What operators must solve next
Discover how AI infrastructure demands system-level design, from power train to thermal chain, in the first episode of DCD AI Week 2026.
Full-stack infrastructure planning for high-density AI deployments
Two data center leaders discuss why treating compute, power, and cooling as a single engineered system is no longer optional as rack densities climb.
Converged physical infrastructure: Moving from components to system outcomes
Converged physical infrastructure integrates power, thermal, and controls as one system for AI-ready data centers. Learn the five non-negotiables for success.
Responsabilidad empresarial
En Vertiv, nos esforzamos por promover los principios de la gestión ambiental, fomentar un lugar de trabajo seguro, inclusivo y comprometido, y llevar a cabo las actividades de nuestro negocio con responsabilidad. Nuestra visión es posibi...
Four dimensions of efficiency: A systems approach to digital infrastructure design
Learn how Vertiv's systems-based approach to data center design embeds efficiency across four key dimensions: energy, water, materials, and carbon management.
AI and safety: How Vertiv embeds protection into every layer of the work
Discover how Vertiv builds safety into every layer of its operations — from daily site huddles to global training — to protect the people powering the AI era.
World Energy Efficiency Day: The AI era’s defining challenge
Discover how integrated power, cooling, and AI-enabled monitoring elevate data center energy efficiency and support scalable, responsible growth in the AI era.
Blog de tecnología
Descubra las ideas, las innovaciones y lo que está dando forma al futuro de la infraestructura digital de Vertiv: desde la alimentación y el enfriamiento hasta el diseño, las operaciones y las tecnologías emergentes.
Precise battery management for AI infrastructure with accurate state of charge (SOC) and state of health (SOH)
AI load spikes don't wait. See why state of charge (SOC) and state of health (SOH) precision is the smarter path to stable, scalable AI power management.
Monitoring and management for liquid-cooled environments
Learn how centralized monitoring and management improve visibility, speeds of response, and support liquid-cooled data center operations.
Serial consoles for driving AI factories’ uptime
Learn why serial console servers can be the only reliable recovery path when hardware fails at hyperscale.
Designing infrastructure for enterprise AI
A decision framework for matching AI workloads to deployment models and physical infrastructure requirements.
Evolución de la cadena térmica
What if cooling wasn’t a single product, but a complete thermal chain?
Explore how data centers are managing the increasing heat loads from high-performance computing (HPC) and artificial intelligence (AI) workloads in this comprehensive guide to modern thermal management strategies, from liquid cooling to heat reuse.
Rethinking heat: A byproduct of useful work and a resource worth capturing
Explore why AI infrastructure is changing how operators view data center heat, from a cooling challenge to a concentrated resource worth capturing.
Navigating the AI cooling challenge: Why hybrid data centers need a smarter approach
Discover how hybrid packaged cooling solutions like the Vertiv™ CoolPhase Flex are helping data center operators navigate the shift to AI workloads — without locking into costly infrastructure decisions too early.
Diseño centrado en lo digital
DCD AI Week 2026: From blueprint to build - Designing smarter with reference architectures and digital twins
Explore from DCD AI Week 2026 how reference architectures and digital twins validate AI factory infrastructure before deployment for data center engineers and operators.
What digital twins reveal about AI infrastructure design
Digital twins are transforming AI data center design by enabling real-time simulation of cooling, power, and electrical systems before construction begins. Learn how Vertiv and NVIDIA Omniverse are advancing physically accurate infrastructure modeling.
Digital twins for operations: Intelligent management
Explore how digital twin technology is moving beyond design validation into real-time operational management of AI data centers — and the financial case for data center operators.
Transformación de la arquitectura de alimentación
La decisión de 800 VCD: Una guía práctica para la arquitectura de alimentación de la IA
Descubra cuándo los 800 VCD tienen sentido para los centros de datos de IA, cómo implementar la adopción por fases y por qué la opcionalidad de la arquitectura es importante.
From rack to data hall: The practical path to 800 VDC
AI rack density is pushing conventional power delivery toward physical limits. Learn how Vertiv is developing a phased 800 VDC architecture from rack-level sidecars to centralized data-hall power.
BESS and UPS roles in large data center power architectures
Learn how UPS and BTM BESS architectures differ, how they work together, and how each supports resilience, flexibility, and AI power smoothing.