The page you're viewing is for Spanish (LATAM) region.

Al trabajar con el soporte de ventas de Vertiv, puede configurar los complejos diseños de acuerdo con sus necesidades específicas. Si forma parte de una organización que busca orientación técnica para un proyecto grande, Vertiv puede ofrecerle el soporte que necesita.

Más información

Muchos clientes trabajan con un socio revendedor de Vertiv para comprar productos de Vertiv para sus aplicaciones de TI. Los socios cuentan con amplia capacitación y experiencia, y están en una posición única para especificar, vender y brindar soporte a soluciones completas de TI e infraestructura con los productos de Vertiv.

Buscar un revendedor

¿Ya sabe lo que necesita? ¿Desea la comodidad de comprar y enviar en línea? Ciertas categorías de productos de Vertiv se pueden comprar a través de un revendedor en línea.


Encontrar un vendedor en línea

¿Necesita ayuda para elegir un producto? Hable con un especialista de Vertiv altamente calificado, quien le guiará hacia la solución adecuada para usted.



Contactar a un especialista de Vertiv

The page you're viewing is for Spanish (LATAM) region.


BUILDINGS has selected the Liebert® DSE with the new optimization feature, released in January 2019, as a 2019 Money-Saving Products winner. This product is a member of an elite group of 65 products showcased online at www.BUILDINGS.com.

Finalists were evaluated by the editorial staff for the money-saving qualities they offer to building owners and facility managers in areas such as energy efficiency, water savings and maintenance.

Now a standard feature on all Liebert DSE systems in North America, and an optional field upgrade to existing field-installed systems, Liebert DSE with optimization provides further energy savings over the previous Liebert DSE product, further reducing power consumption through optimization of the condenser fans, compressors and refrigerant pumps. For instance, applying the optimization upgrade to a 125kW Liebert DSE operating at 50 percent load in San Jose, California, would result in energy savings annually of around 27 percent per unit.

Liebert® DSE is the most efficient water-free data center cooling solution in its class and has more than 6,000 installations. Water use across the data center industry is a growing concern for a variety of reasons, including availability and cost of water, maintenance and upkeep of pumped water systems, and concerns about the proximity of water to sensitive electronics.

Data centers using chilled water systems use approximately 6.75 million gallons of water annually per megawatt capacity, according the Uptime Institute. The Liebert DSE Optimization reduces that number to zero.

About BUILDINGS

BUILDINGS Media serves more than 74,000 commercial building owners and facility managers in North America. Its website, magazine and newsletters provide information that helps subscribers and users make smarter decisions about managing, operating and renovating their facilities.

Artículos relacionados

PRODUCTOS Y SERVICIOS
Descripción general

Idioma y ubicación