Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Emerson Network Power Study Says Unplanned Data Center Outages Cost Companies Nearly $9,000 Per Minute

January 19, 2016

Latest benchmark study from Emerson and Ponemon Institute finds price of downtime continues to climb; average outage cost rose 38 percent in five years

Columbus, Ohio [January 19, 2016] – Emerson Network Power, a business of Emerson (NYSE: EMR) and the world's leading provider of critical infrastructure for information and communications technology systems, in conjunction with the Ponemon Institute, today released the 2016 Cost of Data Center Outages report that estimates the full costs associated with unplanned outages at data centers. Emerson and the Ponemon Institute polled 63 data center organizations in the U.S. that had experienced an outage in the past 12 months.

The two organizations co-released the original Cost of Data Center Outages study, the first independently conducted research on the cost and causes of data center downtime, in 2010. It was updated in 2013 and again this year. Key findings from the new report include:

  • The average total cost per minute of an unplanned outage increased from $5,617 in 2010 to $7,908 in 2013 to $8,851 in this report.
  • The average cost of a data center outage rose from $505,502 in 2010 to $690,204 in 2013 to $740,357 in the latest study. This represents a 38 percent increase in the cost of downtime since the first study in 2010.
  • Maximum downtime costs are rising faster than average, increasing 81 percent since 2010 to a current high of $2,409,991.
  • UPS system failure, including UPS and batteries, is the No. 1 cause of unplanned data center outages, accounting for one-quarter of all such events. Cybercrime represents the fastest growing cause of data center outages, rising from 2 percent of outages in 2010 to 18 percent in 2013 to 22 percent for those sampled in the latest cost of downtime study.

"The complexity of today's data centers continues to create challenges for organizations as they architect and manage their IT infrastructure to reduce costly interruptions," said Steve Hassell, president of data center solutions for Emerson Network Power. "Our goal with the Ponemon Institute research is to provide industry benchmarks and insight that help organizations make smart business decisions to mitigate costly failures."

The Ponemon Institute is recognized in the information technology industry for its independent research on privacy, data protection and information security policy.

This is the first in a series of five research reports from the two organizations that will create industry benchmarks and provide insight into the key challenges and decision points organizations face as they construct an IT infrastructure to support internal users, partners, suppliers and customers in the digital age.

"Emerson laid out a bold challenge to create benchmarks that would better capture the myriad of challenges data center developers and managers face as they support their organizations' digital transformations," said Dr. Larry Ponemon, chairman of the Ponemon Institute.

To download this report and future studies as they become available and view additional supporting content, visit www.EmersonNetworkPower.com/Benchmarks.

About Emerson Network Power
Emerson Network Power, a business of Emerson, is the world's leading provider of critical infrastructure technologies and life cycle services for information and communications technology systems. With an expansive portfolio of intelligent, rapidly deployable hardware and software solutions for power, thermal and infrastructure management, Emerson Network Power enables efficient, highly-available networks. Learn more at www.EmersonNetworkPower.com.

About Emerson
Emerson (NYSE: EMR), based in St. Louis, Missouri (USA), is a global leader in bringing technology and engineering together to provide innovative solutions for customers in industrial, commercial, and consumer markets around the world. The company is comprised of five business segments: Process Management, Industrial Automation, Network Power, Climate Technologies, and Commercial & Residential Solutions. Sales in fiscal 2015 were $22.3 billion. For more information, visit www.Emerson.com.

Media Contact:
Vince McMorrow
614-383-1622
Vince.McMorrow@Fahlgren.com

Partner Login

Language & Location