Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Introduces New, Versatile Power Distribution Offerings for Edge, Colocation, and Mid-Size Data Centers in North America

December 01, 2020

Vertiv™ Liebert® MBX busway and Liebert® TFX power distribution unit provide flexible, user-focused power distribution

 

Columbus, Ohio [Dec. 1, 2020] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today announced AC power distribution offerings that together or singularly will allow data centers to deploy faster, scale easily and operate more reliably. Vertiv™ Liebert® MBX Busway and Vertiv™ Liebert® TFX Power Distribution Unit each provide a modular approach that emphasizes user-focused interfaces and availability for the critical digital equipment. Both offerings are available now in North America.

Rapidly changing capacity demands present challenges to data center managers who face pressure to replace or add equipment quickly and without disruption to the IT load, and often require infrastructure growth without the luxury of additional space. These dynamic environments place a premium on safe, flexible, and reliable power distribution architectures.

“Power distribution today is more critical and more complex than ever before. Technology can play a role in simplifying power distribution to safely enable fast equipment changes and additions,” said Kyle Keeper, vice president of AC power product development and engineering for Vertiv. “Individually, Vertiv Liebert MBX busway and Liebert TFX power distribution unit can simplify and improve reliability for growing data centers. Operating together, they optimize flexibility and efficiency.”

The Vertiv Liebert MBX Busway is ideal for dynamic data center environments that require scalable power distribution to deliver total cost optimization and support adaptation over time as demands change. User friendly tap-off boxes can be placed anywhere along the track for ease of distributing power to equipment racks and feature a ground-first/break-last design with mechanical interlock that ensure user safety. The Liebert MBX Busway supports capacities ranging from 250 to 800 amps and can be configured to support a variety of recepticle options to align with rack PDUs.

To better serve small to mid-sized data centers and colocation facilities, the Vertiv™ Liebert® TFX PDU models deliver 150-300 kVA power in a compact footprint that supports a broad array of installation and landing needs. It can be installed in a corner or against a wall, saving space in tight areas. The transformer-based Liebert TFX PDU offers enhanced Liebert DPM monitoring capabilities for visibility to circuit loads and breaker status via an easy-to-use interface designed for IT and facility managers. The Liebert TFX can be configured for use with busway or remote power panels to support distribution directly to rack PDUs. Isolated panelboards are also available to further enhance the safety of changes and onsite maintenance.

Liebert MBX and Liebert TFX join Vertiv’s broad, industry-leading power distribution portfolio, which includes Liebert® room-based power distribution units (PDUs) and Geist™ rack PDUs. Additional information on power distribution technologies from Vertiv and the entire Vertiv portfolio of solutions for the data center is available at Vertiv.com.

 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. As Architects of Continuity™, Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

 

CONTACT

Sara Steindorf
T (314) 982-1725
E Sara.Steindorf@fleishman.com

PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location