Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Extends Newest Rackmount UPS Line to Support Larger Edge Deployments in North America

September 12, 2019

Vertiv™ Liebert® GXT5 offers higher capacities and voltages, with models up to 10kVA

Columbus, Ohio [Sept. 12, 2019] – Vertiv today announced the addition of new models of the Vertiv™ Liebert® GXT5 family of rackmount, on-line uninterruptible power supply (UPS) systems. The new capacities extend the Liebert GXT5 product ratings with 10 models between 3000VA and 10kVA for higher voltage deployments. The new models are available in 208V only, and refreshed models supporting 208V/120V configurations through Vertiv partners in North America.

Vertiv introduced the Liebert GXT5 in June, updating the 500VA to 3000VA, 120V models of the popular rackmount UPS system. The Liebert GXT5 has a power factor of up to 1.0 on the 5000VA to 10kVA models and is more efficient in both on-line (up to 95 percent) and Active ECO mode (up to 98 percent) than previous models. All Liebert GXT5 models are ENERGY STAR 2.0 certified, and RoHS and REACH compliant.

“The Liebert GXT5 is designed for today’s increasingly critical small IT environments and edge locations, and that includes higher capacity edge sites that demand low latency and high availability to deliver the advanced applications and services today’s users expect,” said Ramesh Menon, vice president of small UPS at Vertiv.

The Liebert GXT5 is the latest addition to the Vertiv channel product portfolio in North America and seamlessly integrates with other products in the portfolio to support single-rack or more complex edge deployments.

The Liebert GXT5 offers scalable runtime options, with additional external battery cabinets that ensure availability even during extended interruptions. It can be managed remotely and has integrated maintenance bypass and flexible output receptacle configurations to meet the connected equipment requirements of any site. When used together with the free Trellis™ Power Insight, users can monitor and manage up to 100 supported Vertiv devices.

Along with the highest level of equipment protection available in a rack configuration, the Liebert® GXT5 offers a three-year full coverage factory warranty for the UPS and battery, a leading warranty in the industry. The system also is available with the Vertiv™ Power Assurance Package, which delivers convenient and cost-effective support for power delivery to small IT sites, and other service packages, to support individual customer needs.

For more information on the Liebert GXT5 UPS, Vertiv and the Vertiv channel program, visit Vertiv.com.

About Vertiv

Vertiv brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs around 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

CONTACT

Vince McMorrow
T +614 383 1622
E Vince.McMorrow@Fahlgren.com

PORTALS
Partner Login

Language & Location