Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Introduces Water-Efficient Liquid Cooling Solution for High-Density Data Centres in EMEA

November 29, 2022

Vertiv™ Liebert® XDU enables liquid cooling for high-performance computing applications, while supporting waste heat recovery and the circular economy

London, UK [November 29, 2022] - Vertiv (NYSE: VRT), today introduced the Liebert® XDU, a new generation of thermal management systems that supports liquid-cooled servers and enables the control of liquid quality, flow and pressure. As high-density computing applications such as data analytics and machine learning increase, rack densities and temperatures are exceeding the cooling capabilities of traditional air-cooled units and require more efficient and sustainable solutions. The Liebert XDU coolant distribution system enables the deployment of liquid cooled server applications into any data centre environment, from core to edge computing sites. The system is now available across Europe, the Middle East and Africa (EMEA).

“High-performance computing applications such as artificial intelligence and augmented reality are growing in popularity at the same time that data centres are working to reduce their energy consumption and pushing the industry to find new, more sustainable solutions,” said Roberto Felisi, senior global director and EMEA business leader for thermal management, Vertiv. “Many colocation providers who have traditionally relied on air cooling are now hosting applications with higher power processors that require more efficient heat management solutions like liquid cooling. With the Vertiv Liebert® XDU, our customers can meet the high-density computing demand whilst improving their operational efficiency.”

The Liebert XDU is an innovative liquid-to-liquid cooling distribution unit available in two capacities, 450kW and a model capable of up to 1368kW, circulating water through liquid-cooled server racks and rejecting the heat from the returning warm water. The system uses a closed water loop to avoid any waste, and is capable of capturing heat to utilize it to warm nearby offices, homes or farms, supporting the circular economy. The Liebert XDU utilizes integrated state-of-the-art controls to vary pump speed to optimize supply water temperature and to provide intelligent flow monitoring and alarms. The compact solution can be placed in the row near the rack it is cooling, or along the room’s perimeter.

Vertiv developed the Liebert XDU in close consultation with data centre operators and server manufacturers, who are deploying ultra-high-density, high-performance computing solutions more frequently across many different types of data centres. The company has defined a strategic roadmap to enhance thermal management technologies that enable liquid cooling adoption as part of its increased investments in research and development.

“Liquid cooling is not a new technology but we’re now seeing a real opportunity in the market to drive more innovative thermal management solutions. The Liebert XDU solution offers the possibility for Vertiv's customers to introduce rack-level liquid cooling and reap the environmental benefits,” said Jon Summers, scientific lead in data centres at RISE - Research Institutes of Sweden. “We look forward to support Vertiv’s R&D roadmap and to combine their engineering excellence with the rigorous analysis and testing capabilities of RISE as part of our ongoing research partnership. This will bring a deeper technical understanding of sustainable and effective approaches for the data centre industry.”

For more information on the Vertiv Liebert XDU and other data centre solutions from Vertiv, visit Vertiv.com or contact your local Vertiv representative.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 24,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

Susanna Collins
T: +44 (0)7872 558593
E: susanna.collins@apodpr.co.uk

PORTALS

Language & Location