When you’re moving the equivalent of the population of Turkey every year in passengers through one airport, it’s a mammoth task to successfully integrate all the interdependent systems. When this airport was forced to cancel thousands of flights over a snowfall, an inquiry was set up to understand how to prevent it happening again.
Command & Control
The outcome of was a directive to create a single future proofed control centre for all 25 departments in one location to detect and manage incident response.
Moving from a legacy control system of four separate control centres, each with double digit numbers of operators, with each operator using more than seven screens and machines at their desks.
Vertiv™ implemented a High Performance KVM solution, which consolidated all data information to Christie video walls. All IT is back-racked in a control room for safety and security
Touch-down
The airport now benefits from rapid resolution of emergency situations through one real-time control centre, powered by Vertiv High performance KVM technology.
Activation status
Please contact Vertiv Partner Support: salescloudsupport@vertivco.com
Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.
Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.
Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.
Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.
How One Airport Went from Failure to Launch to First Class Service
November 03, 2017