Cheque Mate
Banks are strong investors in IT redundancy. For obvious reasons, their reputation is reliant on having strong and secure IT systems, which do not fail.
However, while the Banks datacentres and Branches may live up to this, their more remote ATM machines often fall short of this promise. The result is irritated customers who need money but can’t get it and may need to resort to antiquated methods such as writing a cheque.
Dispensing Help
In the event of an ATM IT failure, the bank often needs to send a person to the machine to restore service because, for example, the network may have failed - this is both costly and time-consuming and not customer friendly.
The right way to manage these eventualities is through the use of an Edge designed Serial Console server which can connect the ATM back to the IT responsible person who can access, diagnose and fix any IT issue relating to the ATM remotely, regardless of whether the network is available. Saving time and money, keeping reputation intact and keeping customers happy.
Activation status
Please contact Vertiv Partner Support: salescloudsupport@vertivco.com
Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.
Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.
Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.
Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.
ACCESS DENIED: How Banks Mitigate ATM IT Failure
10/20/17