Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv delivers space-saving cooling for edge applications, with new ceiling and row systems for North America

2/3/26

The scalable Vertiv™ CoolPhase Ceiling cools with zero footprint, Vertiv™ CoolPhase Row supports high-density row-based equipment

COLUMBUS, Ohio [February 3, 2026] – Vertiv (NYSE: VRT), a global leader in critical digital infrastructure, today announced the expansion of its thermal portfolio with the introduction of the Vertiv™ CoolPhase Ceiling and Vertiv™ CoolPhase Row cooling solutions for edge applications. The ceiling-mounted precision cooling unit is designed for edge computing and small IT spaces, preserving valuable floor space while delivering dedicated cooling for IT equipment. The row-based cooling solution is engineered for high-density data center environments and edge applications, enabling efficient thermal management close to the heat source. The Vertiv CoolPhase Row is available now in North America, while the Vertiv CoolPhase Ceiling will launch in Q2 2026.

“As AI drives more compute to the edge, operators face higher power densities in spaces not built for IT deployments or data center cooling,” said Michal Podmaka, director of Vertiv’s edge thermal product line. “The Vertiv CoolPhase Ceiling and Vertiv CoolPhase Row solutions address these challenges with complementary approaches—delivering targeted overhead and rack-level cooling that integrate seamlessly into Vertiv’s broader thermal chain. Built on Vertiv’s standardized controls and monitoring platforms, they enable consistent visibility and simplified management, to support efficient performance across diverse edge environments.”

Both solutions feature variable-speed components that adjust cooling output to match dynamic heat loads, enabling efficient energy use. Performance and capabilities are certified by AHRI, providing independent assurance of product performance and efficiency. The Vertiv CoolPhase models use R32 refrigerant, a low-global-warming-potential alternative that helps operators meet 2026 environmental standards and offers options for systems to meet future regulatory limits on high-GWP refrigerants, aligning with broader industry and regulatory transitions already underway across global markets. Intelligent Vertiv™ controls and remote monitoring give personnel real-time remote visibility and control, enabling reliable, optimized cooling for IT environments.

The Vertiv CoolPhase Ceiling offers cooling capacities ranging from 3.5 kW to 28 kW. Configurable models are available with customizable options including electric reheat, humidifier, water-side economizers, ducted configurations, or supply/return air grilles, allowing flexibility for various site needs. It provides effective outdoor heat rejection across an extensive temperature range from -31°F to 118°F (-35°C to 48°C), delivering precise temperature control 24/7/365.

The Vertiv CoolPhase Row delivers up to 30kW of cooling capacity in a 11.81 inch (300mm) wide configuration and 40kW of cooling capacity in a 23.62 inch (600mm) wide configuration, maximizing cooling capability while minimizing footprint. The system features dynamic capacity modulation (20-100%) to match real-time IT loads, dual power supply with automatic transfer switching for the condensing unit, teamwork connectivity for active standby control between units, and integrated remote monitoring connection to building management systems. With refrigerant pipe runs up to 295 ft and outdoor heat rejection capability from -31°F to 118°F (-35°C to 48°C), it provides flexible, reliable, and energy-efficient cooling for diverse data center environments.

To learn more about Vertiv’s end-to-end power and thermal management solutions, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-looking statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT
Ruder Finn
E 
Vertiv@RuderFinn.com

Related Articles

PORTALS

Language & Location