Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Technology allows Liebert Series 600T/610 UPS systems to run longer at lower operating temperatures

Columbus, Ohio [July 12, 2017] – Vertiv, formerly Emerson Network Power, now offers a premium capacitor hardening service for the input and output filters of the legacy Liebert® Series 600T/610 uninterruptible power supply (UPS). Capacitor hardening extends capacitor service life for a lower total cost of ownership (TCO). This service is available globally for Liebert Series 600T/610 UPS units ranging from 625 kVA-1 MVA.

This latest service offering was a result of extensive testing and collaboration with SBE Inc., a leading developer of film capacitor solutions. Vertiv adopted SBE’s Power Ring Film Capacitor technology to give customers a replacement option that could better meet their needs. It is ideally suited for UPS units that are 10 years old or newer. Where a traditional electrolytic capacitor might last seven years, the premium capacitors can more than double that lifespan. In some cases, these capacitors last well past 15 years.

“Our premium capacitor hardening service makes for a more reliable and safer capacitor that also extends service life when compared to traditional capacitor technology,” said Dave Saliaris, vice president, Global Lifecycle Management Services, Vertiv. “This offering is a perfect example of our commitment to continuous innovation that will help our customers keep their networks and vital applications running.”

In addition to enabling lower operating temperatures for a longer service life and lower TCO, the technology used in the premium capacitors helps slow down the degradation of surrounding components within the UPS. Since this capacitor design is oil-free, there are also safety benefits, such as the elimination of internal pressure build-up that leads to catastrophic failures and collateral damage.

To learn more about UPS full bank capacitor replacement with premium capacitors and other Vertiv solutions, visit VertivCo.com.


About Vertiv
Vertiv designs, builds and services critical infrastructure that enables vital applications for data centers, communication networks, and commercial and industrial facilities. Formerly Emerson Network Power, Vertiv supports today’s growing mobile and cloud computing markets with a portfolio of power, thermal and infrastructure management solutions including the ASCO®, Chloride®, Liebert®, NetSure™ and Trellis™ brands. Sales in fiscal 2016 were $4.4 billion. For more information, visit VertivCo.com.

 

CONTACT
Vince McMorrow
T +614 383 1622
E Vince.McMorrow@Fahlgren.com

 

PORTALS

Language & Location