Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Does What it Says on the Tin: The IT that Keeps Miners Safe

When a tin mine in Wales had the need to Wi-Fi enable several hundred metres of underground mines to connect with Health and Safety devices and sensors, they faced many issues around placing IT in a hostile environment with no IT expert onsite.

Exploration of One Vendor / One Solution

Starting at the enclosure, Vertiv proposed a durable IP54 rated rack to keep out any dust or moisture, with built-in rack cooling to keep the devices at the right temperature. Next came four hours backup runtime from Vertiv GXT4 UPS in the event of a power outage.

Fissure Free

With no option for break in connectivity, remote serial connectivity, diagnosis and repair to any of the sensors and devices is made possible in the mine by the compact Vertiv ACS800. Top this with FREE Trellis™ Power Insight Software for connection to, and control of the UPS, and the operator had one complete solution to keep miners mining and their operator’s pockets lining. 

Related Articles

PORTALS

Language & Location