First Class Ticket
Signalling systems on transport networks need to remain functioning 24/7. For this, they need robust architecture and redundancy. This solution needs to be able to both diagnose issues quickly and then restore the signalling system fast.
Shunting Yard
Rail networks, having being developed and upgraded over a long time tend to have multiple different technologies of new and old varieties in potentially hostile (hot) and remote environments. This requires an IT system that can talk to all these. Couple that with technical engineering staff who may be based long distances from signalling sites, means the need for remote access is essential for fast restoration of signalling systems.
Coupling Chemistry
Modern rail networks deploy high performance KVM transmitters to the signalling equipment, and corresponding receivers on the operator’s desk so the operator can connect their computer directly into the signalling computer technology and manage it, from a centralised operations centre or any other remote location.
Full Steam Ahead
With over 10,000 miles of track, there are clear opportunities for VAR’s to help either party have safer, more redundant and reliable signalling on the networks.
Activation status
Please contact Vertiv Partner Support: salescloudsupport@vertivco.com
Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.
Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.
Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.
Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.
From Train Wreck to High Spec: Modern IT Mitigates Accidents on Rail Networks
6/15/17