Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Make Sure You’re Up To Speed on the Latest Remote Management Infrastructure

Vertiv™ Avocent® ADX Ecosystem: What You Need to Know

We recently hosted a virtual sales training for the new Vertiv™ Avocent® ADX Ecosystem. If you missed out on the live session, or ever want to refresh on some of the material we covered, you can view an on-demand recording of the training at any time that is convenient for you.

Watch Now

Here are a few key highlights of the training that should encourage your interest in learning more about this new ecosystem of products.  

 

Which customers will be interested in the Avocent® ADX Ecosystem?

Server Engineering Labs Increase efficiency of testing product quality while not requiring an engineer to be on site
Enterprise Development Improve recovery time when a problem occurs because you don’t need to rely on a local staff member to recover critical systems
Remote Working Bank Auditors Enable business continuity with remote workforce to access applications in a secure way
Build-to-Order Factories Improve time to market, save money on travel costs, and minimize the time products spend on shelves
Solution Integration Center Reduce time for provisioning new systems by being able to connect to servers remotely



Products Within the Ecosystem

What’s unique about the Avocent ADX Ecosystem, is that it is not just one single product. It is an ecosystem of products that will fit into the rack that your customers already have at their current data center locations… well isn’t that easy!


MP1000

This part of the ecosystem allows you to manage, control, secure, and automate IT infrastructure from a single platform. Users will benefit from this product by having a simplified management and control of virtual and physical infrastructure, secure and auditable access to devices, and improved efficiency when making changes to their IT devices.

 


RM1048P

This device connects and manages diverse IT devices at the rack while minimizing costs, improving scalability with diverse devices and creating a resilient platform for security, reliability, and high bandwidth demand.

 

 


IPUHD

This device will provide the fastest 4K resolution for your high-resolution needs, with increased productivity for remote access and secure access to remote devices.

 

 


IPIQ

While providing the fast and reliable KVM access from Enterprise to Edge, the IPIQ also provides an extensive amount of benefits including Basic Output/Input System level access without being physically present, improved compression, and end-to-end encryption of all traffic using the latest standards.

 

 

Here are a few helpful resources to help you further your education on the new Avocent ADX Ecosystem.

Related Articles

PORTALS

Language & Location