Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Lithium-Ion Batteries are Energizing Data Centers

Kyle Keeper •

The movement behind lithium-ion batteries (LIB) as an auxiliary energy storage solution for critical applications continues to gain traction.

We at Vertiv have been on the leading edge of this transformation since 2011.  In fact, we are celebrating somewhat of a milestone with over 100MW of lithium-ion batteries deployed with Liebert UPS systems. 

Who is acquiring these systems?  Some are large-scale enterprise customers who have replaced older VRLA (valve-regulated lead-acid) plants which have approached their end of life, some are colocation providers, piloting LIB on one side of their critical bus (while keeping VRLA on the other), and still others are deploying LIB directly into greenfield projects. 

Why are they doing this? Most favor the extended useable life of the battery compared to traditional VRLA. They provide more cycle hits with gradual deterioration, which reduces battery replacement cycles over time, lessening disruption headaches while enhancing availability.   Others desire the smaller size, lower weight ratios against normal VRLA options.  This fact has opened the door to saving space, improving location flexibility and addressing limited floor weight thresholds. 

But, as in any new and transforming practice, there are cautions - one being safety inside a data center.  Not the safety issues seen from handheld electronics, but more the safe application and operation of the solution at your site.  Today, UL and NFPA and others have released codes and standards to assist in the safe utilization of these technologies. The Vertiv paper SAFETY RULES:  An Update of Lithium-ion Battery Use in Critical Facilitiesprovides various comparisons, answers to key questions, chemistry details, and an overview of the major codes you need to know.  Please download a copy here.  

When you are ready to evaluate a LIB solution for an upcoming project, Vertiv experts are ready to help.  Don’t hesitate to contact us. 

  

Feel free to subscribe to our blog to stay informed on the latest trends, technologies and news.

Related Articles

PORTALS

Language & Location