The page you're viewing is for English (LATAM) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (LATAM) region.

How steel-frame modular construction cuts data center embodied carbon by more than half

15 min. Read

New Life Cycle Assessment (LCA) report quantifies the carbon advantage of prefabricated systems over traditional concrete builds and reveals where the savings actually come from.

Download white paper

How you build sets carbon locked in from day one.

While the industry focuses on power usage effectiveness (PUE) and operational efficiency, embodied carbon gets locked in before a single server powers on. And unlike energy consumption, you can't optimize it later.

Data center operators now face converging pressures: accelerating capacity demand, tightening emissions reporting requirements, customer expectations for low-carbon infrastructure, and investor scrutiny of Scope 3 emissions. The task is now to deliver capacity at speed and scale while keeping carbon impact in check.

Prefabricated modular data centers (PMDCs) have gained traction for deployment speed, but their carbon advantage has been more assumed than quantified. Until now.

What the assessment measures

A comprehensive Life Cycle Assessment (LCA) conducted according to European Standard EN 15978 compares "a 1.5-megawatt (MW) PMDC with steel-frame construction" against "a conventional concrete-shell facility with matching IT capacity." The LCA report tracks embodied carbon across material production, transport, construction, refurbishment potential, and end-of-life scenarios.

The scope deliberately excludes operational energy to isolate the carbon impact of construction decisions alone. What remains is a comparison of how building methodology drives the portion of a data center’s carbon footprint that's irreversible once construction begins.

Where prefabricated modular data center wins

The carbon advantage stems from five interconnected factors:

Material efficiency.

Steel-framed modules achieve equivalent structural performance with significantly less material mass than concrete, resulting in lower aggregate emissions.

Factory precision.

Research shows that off-site construction can lower waste to 1.8%, compared to the 30% waste generated by conventional methods.

Efficient, low-impact assembly.

Controlled factory conditions can replace energy-intensive onsite work, cut rework, and streamline logistics. Parallel workstreams can shorten deployment time by up to 50%.

Standardization at scale.

Factory-controlled production environments offer greater measurement precision and consistency.

Steel's circular lifecycle.

Steel maintains its structural integrity through repeated recycling cycles, with "over 90% recovery rates.

Why this study matters

Construction decisions made today will define the industry's carbon trajectory for decades. Understanding how building methodology shapes embodied carbon isn't just about compliance. It's about building infrastructure that scales responsibly.

The full whitepaper includes detailed methodology, life cycle stage analysis, and recommendations for emerging approaches including cross-laminated timber and green steel sourcing.

Get the full analysis, technical specifications, and carbon accounting framework.

Book a meeting modal

<

+

Data center innovation Gigawatt-scale campuses

VertivTM AI Hub

Infrastructure designed to stay multiple compute generations ahead, starting now.

Learn more
Partner Login

Language & Location