Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Vertiv Launches New Line of Compact and Powerful Data Center Cooling Solutions for Edge and Small IT Rooms in Asia, Australia and New Zealand

13/10/21

Singapore [October 13, 2021] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the Vertiv™ Liebert® DM – its latest line of thermal management solutions designed for small and medium-sized computer rooms, IT closets and other edge applications. With capacity ranges from 7 to 27 kW, the Liebert DM is now available across Southeast Asia, Australia, and New Zealand.


Using an intelligent algorithm, the floor-mounted Liebert DM thermal management solution provides enterprise-level cooling features to small computer rooms and network closets, to prevent overheating and downtime of IT equipment. It is designed to provide year-round temperature and humidity control for IT applications. In addition, the Liebert DM features a high sensible heat ratio (SHR) of greater than 0.9, making it ideal for cooling IT environments versus standard comfort cooling solutions.

Vertiv™ Liebert® DM provides year-round
cooling and intelligent controls  

The Liebert DM series is a compact and sensible cooling solution for mission-critical applications such as small IT rooms and edge computing infrastructure in the fields of banking, healthcare, government, transport and energy. This solution is ideal for those that require efficient, reliable and sensible equipment cooling, round-the-clock operation and precise internal environment The Liebert DM can also support battery rooms, and control rooms in industrial and manufacturing applications.

Users have the option to connect up to four units of the Liebert DM series in a single network. With automatic rotation features, multiple Liebert DM units can be installed, configured and synced to ensure optimal management of heat loads in most  IT environments. For example, a customer may opt to install four Liebert DM units in a computer room, and program them to run in a cycle and according to schedule, ensuring equal load distribution and greater efficiency. In addition, built-in emergency features in the Liebert DM will automatically detect any failure, triggering an alarm for immediate action, thus ensuring sufficient cooling.

The Liebert® DM is equipped with user-friendly controls for ease of use, including a 7-inch touchscreen color display as well as real-time, graphical display of return air temperature and relative humidity. The Liebert DM also has built-in intelligent features for added protection, including a three-level password protection and email and SMS notification for remote monitoring functions.

“Many of today’s businesses rely on sophisticated IT processors to enable digital applications in their day-to-day operations. Any failure in these delicate components can lead to potential breakdown and failure, which can have disastrous results. That’s why for these applications, using precision cooling versus comfort cooling is recommended for optimal operation of the IT equipment. The Liebert DM is ideal in this scenario because of its highly efficient and energy-saving features that provide the best cooling versus traditional means,” said Preetam Shah, director for product offering and management for edge thermal solutions, Vertiv Asia & India.

To learn more about Vertiv’s thermal management solutions, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 21,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K/A and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT
Katrina Tirante
T +6326203600 Ext 7666
E Katrina.Tirante@vertiv.com

Reinier Dungca
T +6326203600 Ext 7657
E Reinier.Dungca@vertiv.com

PORTALS
Overview
Partner Login

Language & Location