The page you're viewing is for Japanese (Japan) region.

Vertivの製造担当者と連携すると、複雑な設計をお客様独自のニーズに合わせて構成することが可能になります。大規模なプロジェクトに関する技術的ガイドが必要な組織に対して、Vertivは十分なサポートを提供いたします。

詳細を見る

Vertiv再販業者パートナーと連携して、多くのお客様がITアプリケーション用のVertiv製品を購入しています。パートナーは、広範なトレーニングと経験を積み、ITおよびインフラに関するソリューション全体をVertiv製品で明確にし、販売、サポートを行うという独自の立場を構築しています。

再販業者を見つける

ご自身に必要なものについて特定済みですか? 便利なオンラインショッピングおよび配送をご希望ですか? 特定のカテゴリーのVertiv製品は、オンライン再販業者を通じて購入可能です。


販売代理店のECサイトを検索

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

The page you're viewing is for Japanese (Japan) region.

Designing for performance: Five critical features of row manifold systems in liquid-cooled data centers

4 分 読む

With liquid cooling becoming essential for high-density environments, learn how five key elements contribute to building a resilient and efficient thermal infrastructure for modern data centers.

As data centers increasingly adopt liquid cooling to support high-density compute environments, the infrastructure behind effective coolant distribution becomes just as important as the coolant distribution units (CDUs). At the heart of this infrastructure lies the row manifold system, a critical component responsible for delivering coolant from the CDU to each rack with precision, reliability, and efficiency.

While many manifold systems may appear similar, the difference between a good design and a notable one lies in the details. Here are five essential features that define a high-performing row manifold system and why they matter for long-term success in liquid-cooled deployments.

Material compatibility that protects the entire system

The choice of materials in a manifold system is not just a matter of durability, but also of system integrity. Every surface that comes in contact with coolant must be chemically compatible and corrosion-resistant. Stainless steel, particularly at 304L1 or 316L grade (or higher), has become the industry standard for good reason: it offers excellent resistance to corrosion, supports a wide range of coolants, and aligns with global standards for wetted materials.

Using inferior materials can introduce contaminants, compromise fluid quality, and eventually damage sensitive IT equipment. A well-designed manifold system uses sanitary fittings as a best practice, maintaining a clean, stable environment for coolant flow.

Cleanliness by design

Contaminants in the fluid network—whether from welding residue, pipe tape, or installation debris—can wreak havoc on cold plates and reduce thermal performance. That’s why cleanliness must be engineered in the manifold system from the start.

The best systems arrive passivated, pressure-tested, flushed, dried, and sealed, ready for deployment. Sanitary couplings and pre-assembled modules eliminate the need for on-site fabrication, reducing the risk of introducing foreign materials. This level of cleanliness not only protects the servers but also extends the life of the cooling system and reduces maintenance cycles.

Intelligent flow control for thermal precision

Consistent coolant flow is essential in high-density environments to prevent hotspots and facilitate uniform thermal performance across racks. A well-designed manifold system incorporates advanced flow control features that allow operators to fine-tune the system based on workload and layout.

Various valve types provide granular control over flow rate and pressure. Some even offer integrated energy monitoring, enabling data-driven optimization. Beyond valve control, intelligent flow management also extends to pump regulation. By dynamically adjusting pump speeds based on real-time demand and flow requirements, operators can reduce energy consumption and improve the efficiency of both the pump and the overall cooling system. This level of control secures that the coolant is delivered precisely where and when it's needed, minimizing waste and maximizing thermal performance. These control features are not just conveniences; they are essential for maintaining performance and efficiency at scale.

Modularity that enables speed and flexibility

Data centers are dynamic environments, and cooling infrastructure must be able to keep pace. Modularity in manifold design allows operators to deploy systems quickly, adapt to changing requirements, and scale without disruption.

The most effective systems use standardized header sizes and drip trays, along with a catalog of accessories to further customize the deployment. Whether installed overhead or underfloor, modular manifolds simplify procurement, installation, and future upgrades. This flexibility for customization is especially valuable in the current landscape of varied deployment styles where the needs of enterprise, hyperscale, and everything in between must be met.

Serviceability that minimizes downtime

Even the most resilient systems require maintenance, and serviceability can make or break operational continuity. A well-designed manifold system considers the full lifecycle: from initial concept design to routine maintenance and support.

Quick-disconnect fittings, integrated drip pans, and accessible valve ports make routine maintenance faster and safer. When paired with professional services such as commissioning, fluid analysis, and preventative maintenance, these cooling system design features contribute to its reliability and efficiency over time.

Conclusion

As liquid cooling becomes the standard for high-performance data centers, the design of row manifold systems must evolve to meet the demands of scale, speed, and reliability. The best systems are built with material integrity, engineered cleanliness, intelligent control, modular flexibility, and lifecycle serviceability in mind.

These five features are foundational principles for building a thermal infrastructure that performs under pressure, protects critical assets, and supports the future of compute. Whether you’re designing a hyperscale deployment or a compact edge facility, these are the features that matter most.

1L stands for “low carbon”, signifying carbon content. Regardless of grade, it should be low carbon to prevent the formation of chromium carbide precipitates when welded while maintaining corrosion resistance in the weld area.


サーマルチェーンの進化

VertivTM AI Hub

Infrastructure designed to stay multiple compute generations ahead, starting now.

Learn more
Partner Login

言語と地域