The page you're viewing is for Italian (EMEA) region.

Rivolgiti a un rappresentante di Vertiv che lavorerà al tuo fianco e ti aiuterà a realizzare progetti complessi in base alle tue esigenze. Se la tua organizzazione ha bisogno di assistenza tecnica per un grande progetto, Vertiv può fornirti tutto il supporto necessario.

Ulteriori informazioni

Molti clienti si affidano ai reseller che sono partner di Vertiv per l’acquisto di prodotti ideali per le loro applicazioni IT. Affidati alle elevate competenze dei nostri partner che, grazie ai prodotti Vertiv, sono in grado di offrire soluzioni complete per infrastrutture e applicazioni IT: dalle specifiche alla vendita all’assistenza.

Trova un reseller

Sai già di cosa hai bisogno? Vorresti la comodità dell’acquisto e della spedizione online? Alcune categorie di prodotti Vertiv si possono acquistare tramite un reseller online.


Trova un reseller online

Hai bisogno di aiuto per scegliere un prodotto? Parla con un esperto di Vertiv altamente qualificato che ti orienterà verso la soluzione più adatta.



Contatta un esperto di Vertiv

The page you're viewing is for Italian (EMEA) region.

War Games: The Small Powerful Switch that European Defense Organisations Rely on

Cyber security…yawn!

It’s almost becoming a daily news item of what institution/high profile politician/bank or even Jennifer Lawrence’s iPhone have had data compromised. The public have become largely indifferent to the concept and accept it as a risk of modern life, no more than having your video recorder stolen in the 1980’s by the local thief who spied it in your house.

However, institutions charged with border protection, protecting the welfare and lives of its citizens and military intelligence agencies are far from jaundiced in their interest in the topic.

Obama’s $14bn

Before leaving office, Barack Obama included $14bn for cyber security in the 2016 budget, and still US federal agencies struggle with cyber security. Whether it's phishing, unpatched software, socially engineered trojans or any of the other techniques of cyber terrorists, the weakest link in any organisation is the ability of that hacker, once inside, to be able to roam undetected through the network.

Access denied

To mitigate this risk, what most of these organisations now deploy is what is known as a ‘Secure Switch’ to separate main network access from classified network access. This means that the user has to physically select through the switch which network to use. With the assurance that even if there is a breach in the main network, the hacker cannot ‘jump’ across into the classified network and compromise data.

It's certified

Vertiv’s Secure Desktop Switch with patented “Always-on active anti-tampering system” means that Hardware-based peripheral isolation loads all firmware on ROM with no keyboard buffering or memory.

Governments, Police, Army, Financial Institutions, Healthcare are all vigilant to help protect their reputation. Vertiv’s Switch View Secure helps these organisations protect theirs. 

Login dei partner

Lingua & Ubicazione