Vertiv Emphasizes Commitment to Data Center Lithium-Ion Battery Trend with New Batteries and Cabinet for Large UPS Systems

April 24, 2019

Vertiv HPL rack-based system delivers seamless integration between batteries, monitoring system and UPS

Columbus, Ohio [April 24, 2019] – Vertiv today introduced the Vertiv™ HPL lithium-ion battery cabinet, for use with larger capacity Vertiv uninterruptible power supply (UPS) systems. While Vertiv was an early adopter of lithium-ion batteries for the data center, this marks the first offering with Vertiv’s own battery management system. The cabinet is ready to use with most current and legacy Vertiv three-phase UPS systems and is available in North America and Asia today.

The Vertiv HPL is configured in a cabinet the size of a standard data center rack and ships preassembled with six lithium-ion battery modules. The modular configuration allows for connection of up to eight cabinets to a single UPS in order to customize runtime capacity and redundancy to the application. Vertiv batteries are nickel-manganese-cobalt (NMC), a proven chemistry commonly used for the rigorous standards required for the automobile industry.

“Lithium-ion batteries are increasingly common in the data center, now representing about 30 percent of our deployments worldwide,” said Jeff Kessen, vice president of energy storage at Vertiv. “The Vertiv HPL builds on the inherent benefits of lithium-ion technologies, but goes beyond with features that benefit modern data centers, such as improved user interfaces, integrated controls, and serviceability features that help businesses be more available and competitive.”

Built-in sensors in each battery module and seamless integration with the battery monitoring system allow for real-time monitoring and information at the cell, module, system and facility level. Vertiv HPL allows direct communication between the battery monitoring system within the unit and the external UPS, ensuring early notification of potential issues and maximizing battery life. Redundancy built into the battery management system eliminates single points of failure and ensures high availability of the battery across a range of operating conditions. The Vertiv HPL is warranted to operate up to 86 degrees Fahrenheit (30°C), allowing data center operators to reduce battery cooling costs compared to most alternative solutions.

Lithium-ion batteries are smaller, lighter and last longer than the valve-regulated lead acid (VRLA) batteries traditionally deployed with data center UPS systems. The batteries in the Vertiv HPL have a 10-year battery life guarantee under normal operating conditions. Originally designed and qualified for automobile applications, the batteries meet all existing safety standards and are engineered to comply with evolving fire codes from NFPA.

The Vertiv HPL is compatible with all large Vertiv UPS systems, including the Liebert® EXL, Liebert® EXL S1, the Liebert NX and the Liebert NXL.

Vertiv made the announcement in conjunction with Battcon, which opened Tuesday in Orlando, Florida. For more information on lithium-ion batteries and other products and solutions from Vertiv, visit Vertiv.com.

About Vertiv

Vertiv brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs around 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.  

CONTACT

Vince McMorrow
T +1.614.383.1622

E Vince.McMorrow@Fahlgren.com

Partner Login

Language & Location