The page you're viewing is for English (LATAM) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (LATAM) region.

Adaptive, resilient liquid cooling: How intelligence is upgrading the thermal chain

5 min. Read

Intelligent control holds temperature and flow steady enough to maximize IT output while rejecting the resulting heat with the least energy possible.

AI is forcing a redefinition of cooling control, not just cooling capacity. Liquid cooling is already established as the baseline for high-density AI environments, particularly direct-to-chip (DTC) architectures using liquid-to-air (L2A) and liquid-to-liquid (L2L) approaches. At these densities, a few degrees of drift or a small drop in flow can trigger GPU throttling, and the energy used to reject heat determines cost per megawatt of every workload that runs. Control is what turns liquid cooling from raw capacity into an economic lever.

The components of an intelligent thermal chain

For controls to deliver on this challenge, we embed intelligence across every layer of the thermal chain.

Sensing and visibility

The goal of sensing and visibility is to get as much accurate, real-time sensor data as possible to the appropriate control layer. Sensor capabilities such as auto-discovery and programmatic interfaces make it easier to use sensor data at the local control level or to pass that data on to other components, sub-systems, or full system orchestration layers. The ability to communicate that data, not just collect it, is what enables better AI control loops, full system orchestration, predictive diagnostics, and digital twin development and evolution over time.

AI-driven control loops

With that sensor foundation in place, AI-driven control loops operate across two primary types. The first is unit- and device-embedded control. This type detects operating anomalies such as oscillations within equipment and proactively adjusts control tuning parameters to protect the device from premature failure. Anomaly detection is a core function of this layer. The second is predictive and feed-forward control. This type draws data from sensors, components, and sub-systems beyond the immediate device scope, including AI orchestration systems, power systems, and temperature data from connected devices. The programmatic interfaces and auto-discovery features described above power these capabilities.

System-level orchestration

AI controls deliver their full value when IT, power, and cooling operate as a unified system rather than independent silos. At the thermal chain level, orchestration is about controlling the thermal chain in a way that reduces thermal throttling, connecting individual sub-systems such as the primary and secondary cooling loops so that one sub-system’s data becomes the feed for another, enabling predictive and feed-forward control between them.

Variable-speed pumps, directed by AI, can react to GPU thermal output in real time to maintain stability across the loop. The result is global optimization: breaking down local silos so that sensor data arriving from any point in the system can drive decisions across any connected component or sub-system.

Digital twins as a foundational layer

System-level orchestration delivers its full diagnostic and planning power through digital twins of the data center and its cooling sub-systems. A critical capability of digital twins is that they allow virtual unit and system validation of designs and control algorithms before actual deployment. Before engineers introduce new servers or change rack configurations, they can model the thermal consequences and test control responses in a virtual environment. This is especially valuable in dense AI factory settings where there is very little room for thermal surprises once hardware is in place.

The two critical control challenges

Building the instrumentation and connectivity described above is necessary groundwork. Intelligent controls in liquid-cooled AI environments primarily address two specific challenges:

1. Maintaining liquid loop stability

The first challenge is maintaining stability of fluid flow and temperature across the liquid cooling loop. Effective control depends on synthesizing inputs from multiple sources simultaneously: GPU and server thermal telemetry, power distribution unit (PDU) data, inlet and outlet temperature readings, flow sensors, and coolant quality monitoring.

AI-driven controls must continuously trim pump speeds, modulate valve positions, and hold the loop within its operating parameters. This matters most under rapid load changes, which are characteristic of AI inference workloads. The control logic must be both predictive and fast, because drift in any one parameter, temperature, pressure, or flow rate, can cascade quickly to others.

2. Optimizing the heat rejection loop

The second challenge is translating the state of the liquid loop into effective heat rejection. As AI workloads drive significant and rapid fluctuations in heat output, the heat rejection loop must respond dynamically.

The goal is not only to reject heat, but to maximize efficiency. Intelligent controls continuously evaluate ambient conditions, coolant return temperatures, and load forecasts to determine the optimal heat rejection path, prioritizing economization before shifting to mechanical cooling as needed.

“The combination of full thermal chain data visibility and digital twin AI domain expertise enables global optimization.”

Understanding critical switchover points of the economization and heat rejection sub-systems allows the automated manipulation of controls parameters down the thermal chain providing significant value in not only energy savings but delivered cost per megawatt of AI workload throughout the entire system

This is where load variation connects directly to efficiency outcomes. The more accurately your control system can anticipate load shifts, informed by GPU telemetry and workload scheduling data, the better positioned it is to precondition the heat rejection loop before demand changes arrive. Predictive control is what turns the heat rejection loop into a genuine efficiency asset.

The path forward

Building this capability begins with comprehensive sensor instrumentation across the liquid loop, rack, and facility, followed by integrating IT telemetry, CDU data, and environmental inputs onto a unified platform. From there, we can layer predictive AI controls progressively, starting within specific sub-systems and expanding toward end-to-end automation under human oversight.

An equally important concept shaping this path is modularity. As AI sites scale rapidly, controls must support plug-and-play expansion and allow compute capacity to be added without re-engineering the entire system. The goal is to deliver fully integrated, protected, and optimized building blocks, along with the tools to manage and maintain them as the system scales.

At the same time, this level of system scale and complexity requires stricter governance throughout, with humans able to review, intervene, and override AI decisions at every stage.

Explore how adaptive, resilient liquid cooling is reshaping data center infrastructure in Vertiv Frontiers.


Artificial intelligence Digital-first design Thermal chain evolution Vertiv™ Frontiers
Partner Login

Language & Location