Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Vertiv Expands Liquid Cooling Portfolio with Scalable Solutions for AI And HPC Applications

3/6/25

Now available in EMEA, the expanded Vertiv™ CoolChip CDU family supports any stage of liquid cooling adoption

Cannes, France [June 3, 2025] – Vertiv (NYSE: VRT), a global leader in critical digital infrastructure, today announced the expansion of the Vertiv™ CoolChip CDU (coolant distribution units) family with the launch of the Vertiv™ CoolChip CDU 70, Vertiv™ CoolChip CDU 100 and Vertiv™ CoolChip CDU 600 models in Europe, the Middle East and Africa (EMEA). These direct-to-chip (DTC) liquid cooling solutions enhance Vertiv’s position as a leading innovator and enabler in AI and HPC infrastructure. The Vertiv CoolChip CDU 600 will be showcased for the first time in EMEA at the Vertiv booth at Datacloud Global Congress held this week in Cannes.

“As workloads continue to drive higher rack densities and cooling demands, customers need liquid cooling solutions that adapt to their unique deployment strategies, whether retrofitting an existing environment or scaling a new build,” said Sam Bainborough, vice president, EMEA thermal business at Vertiv. “The Vertiv CoolChip CDU family offers flexible, scalable solutions that simplify deployment and support long-term growth. By reducing integration complexity and adapting to a range of data centre environments, these CDUs help organisations scale liquid cooling more efficiently.”

The new models are designed to suit retrofit or greenfield data centre environments, with models including in-rack and row-based configurations, and liquid-to-air and liquid-to-liquid technologies. The innovative systems offer a flexible, scalable approach to address rising capacity demands while accelerating liquid cooling adoption.

The Vertiv CoolChip CDU family is part of Vertiv’s comprehensive liquid cooling offering and the broader Vertiv™ 360AI portfolio of power, cooling and services that solve the complex challenges of AI deployment. Backed by Vertiv™ Liquid Cooling Services, a global end-to-end offering that supports design, installation, commissioning, fluid management, and maintenance, the liquid cooling portfolio fits in a wide variety of scenarios ranging from retrofitting existing facilities to scaling high-density AI and HPC clusters in new builds.

Vertiv™ CoolChip CDU 70 is an in-row, liquid-to-air coolant distribution unit that enables a fast, cost-effective entry into liquid cooling for data centres retrofitting existing environments or deploying new infrastructure. Designed to utilise existing thermal infrastructure, this liquid-to-air CDU is ideal for facilities looking to deploy liquid cooling capacity without requiring major infrastructure changes. The system delivers up to 70 kW of cooling capacity and is designed for agility and scalability, helping to reduce secondary fluid network complexity and infrastructure footprint. Its integrated controller supports real-time monitoring, group control and unit-to-unit communication, for coordinated thermal performance, simplified management, and efficient scaling across multiple racks.

Vertiv™ CoolChip CDU 100 brings powerful liquid-to-liquid in-rack cooling performance, giving data centres a secure and space-efficient solution for high-density workloads. Ideal for operators to introduce or expand liquid cooling deployments one rack at a time, supporting incremental growth or AI pilot programs without the need for large-scale infrastructure changes. With 100 kW of cooling capacity in a 4U form factor and a large-surface heat exchanger engineered for low approach temperatures, Vertiv CoolChip CDU 100 enables optimal heat transfer. An integrated controller provides monitoring and control capabilities to streamline operations and enhance visibility. Built-in filtration and precise temperature control within ±1°C help maintain fluid quality and thermal stability, while the physical separation of facility and IT loops supports secure, efficient system management in mission-critical environments.

Vertiv™ CoolChip CDU 600 is an in-row, liquid-to-liquid model delivering robust, scalable liquid cooling capacity for high-density AI and HPC deployments. The 600 kW system is designed to meet the demands of hyperscale and colocation environments, supporting in-row configurations and integrating easily into raised floor or retrofit installations. Its design, including top or bottom piping connections and available internal manifolds, streamlines infrastructure planning and speeds implementation. With redundant pumps, advanced monitoring for temperature and fluid quality, and a flexible approach to deployment, Vertiv CoolChip CDU 600 offers reliability, visibility, and performance for customers scaling liquid cooling across broader IT environments.For more information about the Vertiv™ CoolChip CDU family or Vertiv’s end-to-end portfolio of advanced thermal management and power management solutions, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-looking statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

Susanna Collins
T +44 (0)7872 558593
E susanna.collins@apodpr.co.uk

Partner Login

Language & Location