Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Vertiv Expands Liquid Cooling Portfolio with Immersion Cooling Solution for AI and HPC Applications in EMEA

6/11/25

Vertiv™ CoolCenter Immersion is available in 25 – 240kW capacities, delivering highly energy-efficient, scalable liquid cooling for critical applications

LONDON, UK [November 6, 2025] – Vertiv (NYSE: VRT), a global leader in critical digital infrastructure, today introduced the Vertiv™ CoolCenter Immersion cooling system, expanding its global liquid cooling portfolio to support AI and high-performance computing (HPC) environments that are ready to maximise the superior thermal properties of liquid cooling. The system is available now in Europe, the Middle East, and Africa (EMEA).

Immersion cooling submerges entire servers in a dielectric liquid, providing efficient and uniform heat removal across all components, where power densities and thermal loads exceed the limits of traditional air-cooling methods. Vertiv CoolCenter Immersion serves as a complete liquid-cooling architecture, enabling reliable heat removal for dense compute ranging from 25 kW to 240 kW per system. 

“Immersion cooling is playing an increasingly important role as AI and HPC deployments push thermal limits far beyond what conventional systems can handle,” said Sam Bainborough, EMEA vice president of thermal business at Vertiv. “With the Vertiv CoolCenter Immersion, we’re applying decades of liquid-cooling expertise to deliver fully engineered systems that handle extreme heat densities safely and efficiently, giving operators a practical path to scale AI infrastructure without compromising reliability or serviceability.” 

The Vertiv CoolCenter Immersion is available in multiple configurations, including self-contained and multi-tank options, with cooling capacities from 25 kW to 240 kW. Each system includes an internal or external liquid tank, coolant distribution unit (CDU), temperature sensors, variable-speed pumps, and fluid piping, delivering precise temperature control and consistent thermal performance. Dual power supplies and redundant pumps provide high cooling availability, while integrated monitoring sensors, a 9-inch touchscreen, and building management system (BMS) connectivity simplify operation and system visibility. The system’s design also enables heat reuse opportunities, supporting more efficient thermal management strategies across facilities and aligning with broader energy-efficiency objectives.

Vertiv™ Liquid Cooling Services provide end-to-end expertise, from system design and installation to maintenance, training, and lifecycle optimisation, helping customers evaluate and deploy the most effective liquid-cooling architectures. Supported systems include rear-door heat exchangers, direct-to-chip liquid cooling, and immersion cooling, enabling reliable, scalable, and efficient thermal management for AI, HPC, and other high-density computing environments. 

For more information on Vertiv™ CoolCenter Immersion, Vertiv Liquid Cooling Services, and Vertiv’s full portfolio of thermal management, power management, monitoring and management, and integrated solutions, visit Vertiv.com. 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-looking statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT 

Media contact - Vertiv 

susanna.collins@apodpr.co.uk   

Partner Login

Language & Location