Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Vertiv Expands Flexible, Energy-Efficient Perimeter Cooling System for Small, Medium, and Edge Applications in EMEA

21/1/26

Vertiv™ CoolPhase Perimeter PAM low-GWP cooling system features Vertiv™ EconoPhase Pumped Refrigerant Economizer models for EU F-Gas compliance, enhanced safety, and zero-flammability risk

London, UK [21 January 2026] – Vertiv (NYSE: VRT), a global leader in critical digital infrastructure, today enriches the Vertiv™ CoolPhase Perimeter PAM air-cooled range with new ratings of cooling systems and Vertiv™ CoolPhase Condenser. Available now across Europe, the Middle East, and Africa (EMEA), this solution combines energy efficiency, environmental responsibility, and operational resilience, delivering measurable improvements in both power usage effectiveness (PUE) and total cost of ownership (TCO), and helping to extend system lifespan.

Designed for the next generation of data centres, the Vertiv CoolPhase Perimeter PAM now features the highly energy-efficient Vertiv™ EconoPhase Pumped Refrigerant Economizer (PRE), fully integrated into the Vertiv CoolPhase Condenser system. This breakthrough technology aims to reduce energy consumption as it enhances free-cooling and system reliability by using a pumped refrigerant circuit that operates at a fraction of the power required by traditional compressors, while saving space. The Vertiv CoolPhase Perimeter PAM range uses R-513A refrigerant, which features a 70% lower Global Warming Potential (GWP) compared to R-410A, with non-flammability and low toxicity risks. This makes it fully compliant with the EU F-Gas Regulation 2024/573 and ideal for operators seeking to minimise their carbon emissions without compromising cooling performance.

"With this latest addition to the Vertiv CoolPhase Perimeter PAM range, we're making our direct expansion offering more flexible while addressing two critical challenges faced by data centre operators today: environmental compliance and operational efficiency," said Sam Bainborough, VP thermal management, EMEA at Vertiv. "The new air-cooled models boost free-cooling capabilities to lower PUE, demonstrating our commitment to providing energy-efficient and environmentally responsible solutions that don't compromise on performance." 

The Vertiv™ CoolPhase Perimeter PAM range is designed with features such as variable speed compressors, staged coil together with innovative patented filter technology and seamless integration with Vertiv™ CoolPhase Condenser units through Vertiv™ Liebert® iCOM™ control. This is part of a holistic strategy that considers all elements as part of a single system, enabling intelligent optimisation of performance, efficiency and flexibility. 

The Vertiv CoolPhase Perimeter PAM range is part of Vertiv’s thermal chain of products and is backed by the Vertiv™ global service organisation, providing comprehensive support throughout the equipment lifecycle, from design and commissioning to ongoing optimisation, enabling continuous reliability through expert deployment and proactive maintenance.

To learn more about Vertiv’s broad range of thermal, power, IT management and integrated solutions and services, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers' vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today's data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit vertiv.com.

Forward-looking statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

Media contact

Susanna.collins@apodpr.co.uk

Partner Login

Language & Location