Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Vertiv Unveils New Line of Efficient Thermal Management Solutions for High-Density IT Applications in Southeast Asia, Australia and New Zealand

July 08, 2021

The Liebert® XD family features hybrid design configurations for ultimate flexibility and scalability

Singapore [July 8, 2021] Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today unveiled its latest line of thermal management solutions designed for high-density IT applications. The Liebert® XD family offers sensible cooling in row, rack or room design, with provision for scalability and flexibility for future expansion. The Liebert XD family is now available in Southeast Asia, Australia and New Zealand.

The Liebert XD family utilizes refrigerant-based systems to cool IT equipment. By adopting a waterless design, the solution is ideal for use around electrical equipment, reducing hazards and supporting sustainability targets for businesses working to eliminate water usage in the data center.

Ideal for high-density computing applications and enterprise data centers, the Liebert XD family can be implemented as a hybrid approach, using a combination of floormount mission-critical cooling units and cooling from the Liebert XD Series as supplemental or primary. In addition, its compact design allows for targeted cooling closer to the heat source, allowing for potential energy savings of up to 70 percent when deployed as primary cooling and up to 30 percent savings as supplemental cooling, compared to traditional data center cooling solutions.

The Liebert XD family has two types of heat rejection modules available: the Liebert® XDP, which utilizes the building’s existing chilled water system as well as the Liebert XD pumped refrigerant unit, which can cool up to 200kW of IT load; and the Liebert® XDC air-cooled variant, which can support up to 130kW of IT load, for businesses that do not have existing chilled water system in their buildings.

A scalable solution, the Liebert XD cooling solutions may be added and reconfigured to react to changes in the environment as heat loads increase.

The Liebert® XDP and Liebert® XDC units can be used in conjunction with a variety of cooling modules to address unique room cooling challenges: the Liebert® XDH for in-row cooling; the Liebert® XDO for overhead cooling; and the Liebert® XDV for above-rack cooling. Each cooling module supports either air-cooled or chilled water, depending on customer requirements and provision for scalable growth. The cooling modules can be placed where the heat loads are, a flexible approach to provide cooling exactly where it is needed.

“Cooling accounts for one of the biggest energy consumers within the data center space. This is no surprise considering the huge amount of data that’s being processed, stored and analysed as many organizations ramp up their digital transformation programs. As more organizations today strive to balance energy efficiency and sustainability goals with their overall business goals, the Liebert® XD family is the perfect solution to support high-density applications,” said Rebecca Ng, head of thermal management at Vertiv Asia.

To learn more about Vertiv’s thermal management solutions for high-density applications, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs.  Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

Katrina Tirante
T +6326203600 Ext 7666
E Katrina.Tirante@vertiv.com 

Reinier Dungca
T +6326203600 Ext 7657
E Reinier.Dungca@vertiv.com

PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location