Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Vertiv Introduces Upgraded Chilled Water Cooling Solution for High Density and High Compute IT Environments in Asia

17/2/23

The Vertiv™ Liebert® Air Handling Unit (AHU) supports high heat loads with minimal footprint

Singapore [February 16, 2023] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today unveiled the upgraded Vertiv™ Liebert® Air Handling Unit (AHU), a high-capacity, chilled water cooling solution designed to support high-density compute environments, while offering a more energy efficient approach to heat management. The Liebert® AHU has a standard unit capacity of 300kW, and is now available throughout Australia, New Zealand, Southeast Asia and India (ASI) region.

The new Liebert® AHU chilled water unit utilizes water or air-side economizatons and high-efficiency EC fans, working with hot aisle containment to avoid the mixture of supply and return air. The Liebert AHU also operates at higher return air temperature and with higher chilled water temperature, increasing chiller efficiency. With its highly efficient components such as Electronically Commutated (EC) fan, Pressure Independent Control Valve and intelligent controller with multiple remote temperature sensors, the Liebert AHU supplies proper airflow, temperature, and humidity for supported critical IT equipment.

The new model of Liebert AHU is completely chilled water based, and designed with a fan wall configuration that allows for a smoother supply air distribution and higher efficiency hot aisle containment, compared to the previous model. It is designed to achieve the highest standard for fan efficiency of up to 0.2W/CMH. This model has a smaller unit depth, can be modularly installed and is easily serviceable.

The Vertiv™  Liebert® AHU adapts easily to a non-raised floor design simplifying installation, shortening deployment time and reducing associated costs, compared to raised floor systems. The Liebert® AHU cools high-density servers through horizontal air discharge, delivering an even airflow distribution and uniform temperature across the data hall.

The Liebert AHU also allows provision for redundancy or future expansion as it requires no clearance in between units and may be positioned side by side seamlessly. Each unit is built to last and CE Certified for safety and reliability. During maintenance, personnel can access the components from the corridor side and no longer need to enter the data center hall.

The Liebert AHU addresses customers’ needs for a higher-capacity yet compact cooling solution as kW/rack demand continues to increase and data center space is limited, and operates efficiently to combat rising energy costs. Likewise, its modular installation and non-raised floor application makes it an ideal choice for managers aiming to both reduce CAPEX and flexibly deploy cooling units as demand grows.

“Sustainability has become one of the most important points of discussion among organizations today and data center cooling poses a lot of opportunities to optimize energy use. Vertiv’s thermal management systems, including the Liebert AHU, can help reduce energy consumption in the data center and is one of the most effective choices for cooling high density environments,” said Chee Hoe Ling, vice president of infrastructure solutions at Vertiv™ ASI.

 

For more information about Vertiv’s Liebert AHU system and other thermal management solutions, visit Vertiv.com.

 

# # #

 

 

 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

CONTACT

Katrina Tirante
T +6326203600 Ext 7666
E Katrina.Tirante@vertiv.com

Reinier Dungca
T +6326203600 Ext 7657
E Reinier.Dungca@vertiv.com

PORTALS
Overview
Partner Login

Language & Location