Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Vertiv Expands Data Center Thermal Management Portfolio with New High Density Chilled Water Model for Southeast Asia, Australia and New Zealand

2/2/22

Developed by Vertiv’s own research and development team using the latest technologies and performance tested in a GMPI Certified Laboratory, the Liebert PCW’s coil design and airflow optimization enables it to support high capacities in a compact footprint, to deliver best-in-class cooling performance.

Singapore [February 2, 2022] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, continues to expand its data center thermal management product portfolio with the launch of the expanded Liebert® PCW chilled water range. Designed for medium to large-scale data centers and to support high-density computing, the Liebert PCW now offers up to 250kW of cooling capacity and is available throughout Southeast Asia, Australia and New Zealand.

 

The Liebert® PCW can deliver up to 250kW cooling for medium to large data centers

Developed by Vertiv’s own research and development team using the latest technologies and performance tested in a GMPI Certified Laboratory, the Liebert PCW’s coil design and airflow optimization enables it to support high capacities in a compact footprint, to deliver best-in-class cooling performance. Moreover, with the expanded capacity of up to 250kW, the Liebert PCW is able to deliver more cooling power with less footprint due to its space-saving and compact design, while also supporting high return air temperatures and chilled water temperatures for improved efficiency. The family offers other models in capacities from 69.7 to 208.9 KW.

The new PH250 model in the Liebert PCW series has three air flow configrations: down flow and new front and rear supply for non-raised floor applications. The new front and rear flow configurations allow for large airflow capability with no raised floor, bringing customer savings in construction time and operating costs versus adapting to a raised floor installation.

Each Liebert PCW unit comes equipped with the new EBM RadiCal centrifugal fan with EC motor, which delivers optimum cooling with minimum power consumption. Additionally, the integrated Liebert® iCOM controller has a new touch screen with a complete view of status in single screen, allowing operators to make quick and precise decisions on unit performance.

“As the world continues its digital transformation, the overall market for larger data centers is growing. Additionally, data centers have to be agile and deployed quickly. The release of the expanded Liebert PCW range will give our customers the added flexibility to support high-density computing applications while meeting their efficiency goals through energy savings. This will certainly address the needs of medium to large scale data centers in the region,” said Rebecca Ng, head of thermal management at Vertiv in Asia.

Vertiv continues to provide innovative thermal management solutions to address the needs of its customers in the region. Among the other thermal management solutions launched this year are the Liebert® VIC liquid immersion cooling solution, the Liebert® XD family for high heat densities, and the Liebert® DM room cooling for small and medium data centers.

To learn more about Vertiv’s thermal management solutions, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 21,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K/A and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

Katrina Tirante
T +6326203600 Ext 7666
E Katrina.Tirante@vertiv.com

Reinier Dungca
T +6326203600 Ext 7657
E Reinier.Dungca@vertiv.com

PORTALS
Overview
Partner Login

Language & Location