Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Vertiv Announces New Line of High-Definition,
IP-Based Signal Extender for Control Rooms in Asia Pacific

21/9/22

Vertiv™ HMX 3080/4080 IP-based KVM provides 1080p high-quality video with ultra-fast switching capabilities.

Singapore [September 21, 2022] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the Vertiv™ Avocent® HMX 3080/4080 series, an IP-based signal extender allowing users to remotely transmit DVI video, audio, USB and RS232 signals over a Gigabit network. The product is available now, exclusively in Greater China, South East Asia, Australia, New Zealand and India.

The Vertiv Avocent HMX 3080/4080 series joins the company’s high performance IP-based KVM portfolio. It improves from the Avocent® HMX 1080/2080 series with the below key benefits:

 

Key Benefits

  • Enhanced Performance: Comprising transmitter and receiver units, each device is assigned a unique IP address to help mitigate KVM transmission losses.
  • Flexible Architecture: The desktop-based Avocent HMX 3080/4080 offers multiple connectivity options. The receiver and transmitters can be directly connected using CATx and fiber cables. Using the integrated network ports, a single transmitter can be connected to multiple receivers or vice versa, and for connectivity redundancy.
  • Virtual IP Matrix: With sufficient bandwidth and network switch ports, an IP matrix architecture can support up to 65,000 receivers in the same network.
  • Ease of Use: Any receiver terminal in the network can autodetect and configure all the devices in the network.

The Avocent HMX 3080/4080 is ideal for control room settings in broadcast, emergency management, industrial, and energy organizations that require high-definition video and high quality audio. 

For more information on the Vertiv Avocent HMX 3080/4080 series and the full portfolio of Vertiv IT management solutions, visit Vertiv.com.

 

 

# # #

 

 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 24,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

 

CONTACT
Katrina Tirante
T +6326203600 Ext 7666
E Katrina.Tirante@vertiv.com

Reinier Dungca
T +6326203600 Ext 7657
E Reinier.Dungca@vertiv.com

 

PORTALS
Overview
Partner Login

Language & Location